<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32Kのトピックemios trigger</title>
    <link>https://community.nxp.com/t5/S32K/emios-trigger/m-p/1968889#M41773</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am trying to test the system so that the BCTU is triggered via PWM&amp;nbsp; at every flag generation. I would like to plot the flag that triggers the BCTU on an oscilloscope. How do I do that?&lt;/P&gt;&lt;P&gt;I am trying to get the generating emios_pwm flag outputted on an oscilloscope, by using the EMIOS_PWM_IP_INTERRUPT_REQUEST callback function, but i am not sure the interrupt for EMIOS is working. I have attached the project below&lt;/P&gt;&lt;P&gt;RTD 4.00&lt;/P&gt;&lt;P&gt;S32K344 T172&lt;/P&gt;</description>
    <pubDate>Tue, 08 Oct 2024 11:57:58 GMT</pubDate>
    <dc:creator>Ayaz</dc:creator>
    <dc:date>2024-10-08T11:57:58Z</dc:date>
    <item>
      <title>emios trigger</title>
      <link>https://community.nxp.com/t5/S32K/emios-trigger/m-p/1968889#M41773</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am trying to test the system so that the BCTU is triggered via PWM&amp;nbsp; at every flag generation. I would like to plot the flag that triggers the BCTU on an oscilloscope. How do I do that?&lt;/P&gt;&lt;P&gt;I am trying to get the generating emios_pwm flag outputted on an oscilloscope, by using the EMIOS_PWM_IP_INTERRUPT_REQUEST callback function, but i am not sure the interrupt for EMIOS is working. I have attached the project below&lt;/P&gt;&lt;P&gt;RTD 4.00&lt;/P&gt;&lt;P&gt;S32K344 T172&lt;/P&gt;</description>
      <pubDate>Tue, 08 Oct 2024 11:57:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/emios-trigger/m-p/1968889#M41773</guid>
      <dc:creator>Ayaz</dc:creator>
      <dc:date>2024-10-08T11:57:58Z</dc:date>
    </item>
    <item>
      <title>Re: emios trigger</title>
      <link>https://community.nxp.com/t5/S32K/emios-trigger/m-p/1969831#M41844</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@Ayaz" target="_blank"&gt;Hi@Ayaz&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;This is a demo i made before and the RTD version is 2.0.3, maybe you can refer to it.&lt;/P&gt;</description>
      <pubDate>Wed, 09 Oct 2024 10:02:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/emios-trigger/m-p/1969831#M41844</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2024-10-09T10:02:13Z</dc:date>
    </item>
  </channel>
</rss>