<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic s32K312 MCAL RTE SchM Core Number in S32K</title>
    <link>https://community.nxp.com/t5/S32K/s32K312-MCAL-RTE-SchM-Core-Number/m-p/1967577#M41670</link>
    <description>&lt;P&gt;C:\NXP\SW32K3_S32M27x_RTD_R21-11_5.0.0\eclipse\plugins\Rte_TS_T40D34M50I0R0\include\SchM_Adc.h&lt;/P&gt;&lt;P&gt;The core number is declared as 4 in the file above.&lt;BR /&gt;Is there a special reason why it is fixed to 4 and not defined separately for each MCU?&lt;BR /&gt;Do I need to change it manually if I use S32K312?&lt;/P&gt;</description>
    <pubDate>Mon, 07 Oct 2024 04:55:19 GMT</pubDate>
    <dc:creator>kjy106906</dc:creator>
    <dc:date>2024-10-07T04:55:19Z</dc:date>
    <item>
      <title>s32K312 MCAL RTE SchM Core Number</title>
      <link>https://community.nxp.com/t5/S32K/s32K312-MCAL-RTE-SchM-Core-Number/m-p/1967577#M41670</link>
      <description>&lt;P&gt;C:\NXP\SW32K3_S32M27x_RTD_R21-11_5.0.0\eclipse\plugins\Rte_TS_T40D34M50I0R0\include\SchM_Adc.h&lt;/P&gt;&lt;P&gt;The core number is declared as 4 in the file above.&lt;BR /&gt;Is there a special reason why it is fixed to 4 and not defined separately for each MCU?&lt;BR /&gt;Do I need to change it manually if I use S32K312?&lt;/P&gt;</description>
      <pubDate>Mon, 07 Oct 2024 04:55:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32K312-MCAL-RTE-SchM-Core-Number/m-p/1967577#M41670</guid>
      <dc:creator>kjy106906</dc:creator>
      <dc:date>2024-10-07T04:55:19Z</dc:date>
    </item>
    <item>
      <title>Re: s32K312 MCAL RTE SchM Core Number</title>
      <link>https://community.nxp.com/t5/S32K/s32K312-MCAL-RTE-SchM-Core-Number/m-p/1993539#M43217</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/187044"&gt;@kjy106906&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The define is indicating the maximum core number for the maximal derivative from the family as the memmap files are generic stubs. The actual core number used at runtime is based on the value provided by Osif so it will use the correct core in execution.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1731488690903.png" style="width: 448px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/310236iAD27D6B63E9A8D3F/image-dimensions/448x45?v=v2" width="448" height="45" role="button" title="danielmartynek_0-1731488690903.png" alt="danielmartynek_0-1731488690903.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Wed, 13 Nov 2024 09:09:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32K312-MCAL-RTE-SchM-Core-Number/m-p/1993539#M43217</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2024-11-13T09:09:11Z</dc:date>
    </item>
  </channel>
</rss>