<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K MCAL generate error in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K-MCAL-generate-error/m-p/1965138#M41503</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;it just says that you should have HTH (transmit handlers) Ids higher then HRH (receive handlers) Ids. So try to &lt;SPAN&gt;place the HRH before HTH as in the below image:&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="CanObjectId HRH HTH There must not be HTH with Object ID lower than that of any HRH configured.png" style="width: 916px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/302195i2DA95852BB5CB829/image-size/large?v=v2&amp;amp;px=999" role="button" title="CanObjectId HRH HTH There must not be HTH with Object ID lower than that of any HRH configured.png" alt="CanObjectId HRH HTH There must not be HTH with Object ID lower than that of any HRH configured.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;CanObjectId HRH HTH There must not be HTH with Object ID lower than that of any HRH configured.png&lt;/span&gt;&lt;/span&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR, Petr&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 01 Oct 2024 11:20:13 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2024-10-01T11:20:13Z</dc:date>
    <item>
      <title>S32K MCAL generate error</title>
      <link>https://community.nxp.com/t5/S32K/S32K-MCAL-generate-error/m-p/1964128#M41440</link>
      <description>&lt;P&gt;When I use tresos to generate the cfg for CAN, a error is reported as below: [C:\EB\Tresos\..\..\NXP\AUTOSAR\S32K1XX_MCAL4_3_RTM_1_0_5\eclipse\plugins\Can_TS_T40D2M10I5R0/generate_PB/src/Can_PBcfg.c (signed):237]: The HRH and HTH Ids are defined under two different name-spaces (Refer to CAN326). Example: HRH0-0, HRH1-1, HTH0-2, HTH1-3. The HRHs of all controllers are grouped before the HTHs of all controllers (there must not be any HTH of any controller with an object ID lower than that of any HRH configured for this driver). (node )&lt;/P&gt;&lt;P&gt;Could you help confirm the problem if my configuration is wrong&lt;/P&gt;</description>
      <pubDate>Mon, 30 Sep 2024 03:37:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-MCAL-generate-error/m-p/1964128#M41440</guid>
      <dc:creator>BarryQi</dc:creator>
      <dc:date>2024-09-30T03:37:47Z</dc:date>
    </item>
    <item>
      <title>Re: S32K MCAL generate error</title>
      <link>https://community.nxp.com/t5/S32K/S32K-MCAL-generate-error/m-p/1965138#M41503</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;it just says that you should have HTH (transmit handlers) Ids higher then HRH (receive handlers) Ids. So try to &lt;SPAN&gt;place the HRH before HTH as in the below image:&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="CanObjectId HRH HTH There must not be HTH with Object ID lower than that of any HRH configured.png" style="width: 916px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/302195i2DA95852BB5CB829/image-size/large?v=v2&amp;amp;px=999" role="button" title="CanObjectId HRH HTH There must not be HTH with Object ID lower than that of any HRH configured.png" alt="CanObjectId HRH HTH There must not be HTH with Object ID lower than that of any HRH configured.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;CanObjectId HRH HTH There must not be HTH with Object ID lower than that of any HRH configured.png&lt;/span&gt;&lt;/span&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR, Petr&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 01 Oct 2024 11:20:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-MCAL-generate-error/m-p/1965138#M41503</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-10-01T11:20:13Z</dc:date>
    </item>
  </channel>
</rss>