<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 s32k3 eMIOS IMP Mode</title>
    <link>https://community.nxp.com/t5/S32K/s32k3-eMIOS-IMP-Mode/m-p/1964561#M41477</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm currently trying to read in an input signal frequency using eMIOS IPM mode on an s32k3 micro. After I wait for the Status register to tell me it's captured a measurement, I read the A register first, then the B register, and perform the period calculation for both cases (Normal case, and overflow case). However, the calculation instead gives me either the "High Time" or the "Low time", not the period of the signal. It appears that the IPM mode is giving me the high/low duty cycle instead of the period. Any thoughts to figure this out? I've confirmed the Control register is using the correct mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Mon, 30 Sep 2024 14:49:49 GMT</pubDate>
    <dc:creator>jfranklin</dc:creator>
    <dc:date>2024-09-30T14:49:49Z</dc:date>
    <item>
      <title>s32k3 eMIOS IMP Mode</title>
      <link>https://community.nxp.com/t5/S32K/s32k3-eMIOS-IMP-Mode/m-p/1964561#M41477</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm currently trying to read in an input signal frequency using eMIOS IPM mode on an s32k3 micro. After I wait for the Status register to tell me it's captured a measurement, I read the A register first, then the B register, and perform the period calculation for both cases (Normal case, and overflow case). However, the calculation instead gives me either the "High Time" or the "Low time", not the period of the signal. It appears that the IPM mode is giving me the high/low duty cycle instead of the period. Any thoughts to figure this out? I've confirmed the Control register is using the correct mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Mon, 30 Sep 2024 14:49:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k3-eMIOS-IMP-Mode/m-p/1964561#M41477</guid>
      <dc:creator>jfranklin</dc:creator>
      <dc:date>2024-09-30T14:49:49Z</dc:date>
    </item>
    <item>
      <title>Re: s32k3 eMIOS IMP Mode</title>
      <link>https://community.nxp.com/t5/S32K/s32k3-eMIOS-IMP-Mode/m-p/1964802#M41490</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/241289"&gt;@jfranklin&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Are you using RTD controllers or custom software? Could you provide us with more information about your application?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
      <pubDate>Mon, 30 Sep 2024 22:00:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k3-eMIOS-IMP-Mode/m-p/1964802#M41490</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2024-09-30T22:00:49Z</dc:date>
    </item>
    <item>
      <title>Re: s32k3 eMIOS IMP Mode</title>
      <link>https://community.nxp.com/t5/S32K/s32k3-eMIOS-IMP-Mode/m-p/1965250#M41510</link>
      <description>&lt;P&gt;Hi, it's our own software. Our goal is to not use the gui that's provided. Basically I'm just trying to read the period of a frequency input. It seems that even though IPM mode should only update on only rising or only falling edges, it seems to be updating on both rising and falling.&lt;/P&gt;</description>
      <pubDate>Tue, 01 Oct 2024 14:05:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k3-eMIOS-IMP-Mode/m-p/1965250#M41510</guid>
      <dc:creator>jfranklin</dc:creator>
      <dc:date>2024-10-01T14:05:36Z</dc:date>
    </item>
    <item>
      <title>Re: s32k3 eMIOS IMP Mode</title>
      <link>https://community.nxp.com/t5/S32K/s32k3-eMIOS-IMP-Mode/m-p/1965860#M41563</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/241289"&gt;@jfranklin&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If possible could you share your configurations?&lt;/P&gt;</description>
      <pubDate>Wed, 02 Oct 2024 17:32:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k3-eMIOS-IMP-Mode/m-p/1965860#M41563</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2024-10-02T17:32:28Z</dc:date>
    </item>
    <item>
      <title>Re: s32k3 eMIOS IMP Mode</title>
      <link>https://community.nxp.com/t5/S32K/s32k3-eMIOS-IMP-Mode/m-p/2291355#M56037</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201913"&gt;@VaneB&lt;/a&gt;&amp;nbsp;Hi,&lt;BR /&gt;I'm also facing similar problems can you share the configuration like how i can&amp;nbsp; configure the EMIOS for the measuring the frequency.&lt;/P&gt;</description>
      <pubDate>Sun, 11 Jan 2026 04:47:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k3-eMIOS-IMP-Mode/m-p/2291355#M56037</guid>
      <dc:creator>gayancho</dc:creator>
      <dc:date>2026-01-11T04:47:31Z</dc:date>
    </item>
  </channel>
</rss>