<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K324 Single and specific Core Reset issue in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K324-Single-and-specific-Core-Reset-issue/m-p/1963660#M41412</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/230626"&gt;@ivaneo1979&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I see you have also created an internal case. I will continue to support you through the case in order to avoid any confusions.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
    <pubDate>Fri, 27 Sep 2024 16:15:13 GMT</pubDate>
    <dc:creator>Julián_AragónM</dc:creator>
    <dc:date>2024-09-27T16:15:13Z</dc:date>
    <item>
      <title>S32K324 Single and specific Core Reset issue</title>
      <link>https://community.nxp.com/t5/S32K/S32K324-Single-and-specific-Core-Reset-issue/m-p/1962549#M41367</link>
      <description>&lt;P&gt;Good morning,&lt;/P&gt;&lt;P&gt;I´m exploring the possibility to re-start a specific core, i.e. the main core wants to stop and completely restart the application core.&lt;/P&gt;&lt;P&gt;I successfully implemented both&amp;nbsp;Application core initialization process and the Application Core shutdown process (46.1.6/7 in S32K3xx Ref.Manual).&lt;/P&gt;&lt;P&gt;This means that Core 0 can start Core 1 and can Stop it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;However what I need is the possibility to completely restart the Core 1 after stopping it.&lt;/P&gt;&lt;P&gt;Try to explain: Core 1 Stop means that it remains in "standby" and waiting-for-interrupt (WFI), once this is triggered it carries on with the normal runtime flow BUT what I need it is to completely restart Core 1, i.e. I need a clean reset of a single Core.&lt;/P&gt;&lt;P&gt;Is that possible? I couldn´t find any way so far to implement this feature.&lt;/P&gt;</description>
      <pubDate>Thu, 26 Sep 2024 09:11:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K324-Single-and-specific-Core-Reset-issue/m-p/1962549#M41367</guid>
      <dc:creator>ivaneo1979</dc:creator>
      <dc:date>2024-09-26T09:11:47Z</dc:date>
    </item>
    <item>
      <title>Re: S32K324 Single and specific Core Reset issue</title>
      <link>https://community.nxp.com/t5/S32K/S32K324-Single-and-specific-Core-Reset-issue/m-p/1963660#M41412</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/230626"&gt;@ivaneo1979&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I see you have also created an internal case. I will continue to support you through the case in order to avoid any confusions.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
      <pubDate>Fri, 27 Sep 2024 16:15:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K324-Single-and-specific-Core-Reset-issue/m-p/1963660#M41412</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-09-27T16:15:13Z</dc:date>
    </item>
  </channel>
</rss>