<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K312 LPUART Problem in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K312-LPUART-Problem/m-p/1963360#M41404</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Please refer to the examples:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-UART-Transmit-amp-Receive-Using-Interrupt-DS3-5/ta-p/1818775" target="_self"&gt;Example S32K312 UART Transmit &amp;amp; Receive Using Interrupt DS3.5 RTD300&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-UART-Transmit-amp-Receive-Using-DMA-DS3-5-RTD300/ta-p/1787799" target="_self"&gt;Example S32K312 UART Transmit &amp;amp; Receive Using DMA DS3.5 RTD300&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Fri, 27 Sep 2024 07:52:34 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2024-09-27T07:52:34Z</dc:date>
    <item>
      <title>S32K312 LPUART Problem</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-LPUART-Problem/m-p/1963265#M41400</link>
      <description>&lt;P&gt;when i send data use :&lt;/P&gt;&lt;P&gt;Lpuart_Uart_Ip_AsyncSend(UART2,frm-&amp;gt;write_array, NEX13120_LEN_Write_data_Length1);&lt;/P&gt;&lt;P&gt;the MCU will enter :undefined_handler.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xingjunwei_0-1727418297734.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/301629i71899639310007D9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xingjunwei_0-1727418297734.png" alt="xingjunwei_0-1727418297734.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xingjunwei_0-1727418297734.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 27 Sep 2024 06:25:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-LPUART-Problem/m-p/1963265#M41400</guid>
      <dc:creator>xingjunwei</dc:creator>
      <dc:date>2024-09-27T06:25:27Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 LPUART Problem</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-LPUART-Problem/m-p/1963360#M41404</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Please refer to the examples:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-UART-Transmit-amp-Receive-Using-Interrupt-DS3-5/ta-p/1818775" target="_self"&gt;Example S32K312 UART Transmit &amp;amp; Receive Using Interrupt DS3.5 RTD300&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-UART-Transmit-amp-Receive-Using-DMA-DS3-5-RTD300/ta-p/1787799" target="_self"&gt;Example S32K312 UART Transmit &amp;amp; Receive Using DMA DS3.5 RTD300&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 27 Sep 2024 07:52:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-LPUART-Problem/m-p/1963360#M41404</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-09-27T07:52:34Z</dc:date>
    </item>
  </channel>
</rss>