<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32k322_MCAL_GPT</title>
    <link>https://community.nxp.com/t5/S32K/S32k322-MCAL-GPT/m-p/1960827#M41294</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;so you measure periodic signal with desired period, so you must toggle pin in your code at that rate based on GPT notification. But then you wrote it is not triggering continuously. How does that relates?&lt;BR /&gt;Can you share full code you have?&lt;BR /&gt;Within RTD there is GPT demo using PIT timer, this would be better for periodic interrupt functionality, I think.&lt;/P&gt;
&lt;P&gt;BR, Petr&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 24 Sep 2024 13:56:50 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2024-09-24T13:56:50Z</dc:date>
    <item>
      <title>S32k322_MCAL_GPT</title>
      <link>https://community.nxp.com/t5/S32K/S32k322-MCAL-GPT/m-p/1958786#M41194</link>
      <description>&lt;P&gt;I am using s32k322 board ,and EB tresos version 29.0&lt;/P&gt;&lt;P&gt;I am using MCAL Package&amp;nbsp;SW32K3_S32M27x_RTD_4.4_4.0.0_P24&lt;/P&gt;&lt;P&gt;I want to create a 20 ms delay. The STM Input clock frequency is 80 MHz, and the tick count is 1,600,000 with a prescaler of 1. I need to validate the GPT (General Purpose Timer) functionality.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="BalasubramaniyanS_2-1726833349798.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/300391i58FE9F8CABCF4BCE/image-dimensions/632x60?v=v2" alt="BalasubramaniyanS_2-1726833349798.png" title="BalasubramaniyanS_2-1726833349798.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But when I checked the logic analyzer, I was getting the correct 20 ms.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="BalasubramaniyanS_1-1726833313852.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/300390iD6DC9BD77F16EC8C/image-size/medium?v=v2&amp;amp;px=400" alt="BalasubramaniyanS_1-1726833313852.png" title="BalasubramaniyanS_1-1726833313852.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, the interrupt is occurring twice and hitting with a delay, but it’s not triggering continuously.&lt;/P&gt;</description>
      <pubDate>Fri, 20 Sep 2024 12:05:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k322-MCAL-GPT/m-p/1958786#M41194</guid>
      <dc:creator>BalasubramaniyanS</dc:creator>
      <dc:date>2024-09-20T12:05:24Z</dc:date>
    </item>
    <item>
      <title>Re: S32k322_MCAL_GPT</title>
      <link>https://community.nxp.com/t5/S32K/S32k322-MCAL-GPT/m-p/1960827#M41294</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;so you measure periodic signal with desired period, so you must toggle pin in your code at that rate based on GPT notification. But then you wrote it is not triggering continuously. How does that relates?&lt;BR /&gt;Can you share full code you have?&lt;BR /&gt;Within RTD there is GPT demo using PIT timer, this would be better for periodic interrupt functionality, I think.&lt;/P&gt;
&lt;P&gt;BR, Petr&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 24 Sep 2024 13:56:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k322-MCAL-GPT/m-p/1960827#M41294</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-09-24T13:56:50Z</dc:date>
    </item>
  </channel>
</rss>