<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Compatibility issue between S32K344 and S32K324 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Compatibility-issue-between-S32K344-and-S32K324/m-p/1960111#M41259</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/230296"&gt;@Chenxu1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;1. Can S32K324 and S32K344 be obtained from each other by decoupling and locking steps? (mass production phase)&lt;/STRONG&gt;&lt;BR /&gt;It is not possible because the production MCU comes with this feature locked.&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;2. Can the project be downloaded from S32K324 to S32K344?&lt;/STRONG&gt;&lt;BR /&gt;It is not possible because there are several settings made in the project that will cause failures on other devices different than the version for which the project was created.&amp;nbsp;I am afraid that the most viable option is to generate a new project with the corresponding MCU and then copy the application source files from your pre-existing project as well as any customizations you made to the project properties.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
    <pubDate>Mon, 23 Sep 2024 19:45:03 GMT</pubDate>
    <dc:creator>VaneB</dc:creator>
    <dc:date>2024-09-23T19:45:03Z</dc:date>
    <item>
      <title>Compatibility issue between S32K344 and S32K324</title>
      <link>https://community.nxp.com/t5/S32K/Compatibility-issue-between-S32K344-and-S32K324/m-p/1958539#M41175</link>
      <description>&lt;P&gt;Hi，I have encountered the following problems recently, please help to answer , thanks.&lt;BR /&gt;&lt;BR /&gt;1、Can S32K324 and S32K344 be obtained from each other by decoupling and locking steps?（mass production phase）&lt;BR /&gt;&lt;BR /&gt;At present, P32K344 and P32K324（sample stage） of my test&amp;nbsp; are able to free to decouple and lock step.&lt;BR /&gt;&lt;BR /&gt;2、Can S32K324's project be downloaded to S32K344?&amp;nbsp; If so，what needs to be changed?&lt;BR /&gt;&lt;BR /&gt;Expecting a reply.&amp;nbsp; TKS.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 20 Sep 2024 08:02:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Compatibility-issue-between-S32K344-and-S32K324/m-p/1958539#M41175</guid>
      <dc:creator>Chenxu1</dc:creator>
      <dc:date>2024-09-20T08:02:26Z</dc:date>
    </item>
    <item>
      <title>Re: Compatibility issue between S32K344 and S32K324</title>
      <link>https://community.nxp.com/t5/S32K/Compatibility-issue-between-S32K344-and-S32K324/m-p/1960111#M41259</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/230296"&gt;@Chenxu1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;1. Can S32K324 and S32K344 be obtained from each other by decoupling and locking steps? (mass production phase)&lt;/STRONG&gt;&lt;BR /&gt;It is not possible because the production MCU comes with this feature locked.&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;2. Can the project be downloaded from S32K324 to S32K344?&lt;/STRONG&gt;&lt;BR /&gt;It is not possible because there are several settings made in the project that will cause failures on other devices different than the version for which the project was created.&amp;nbsp;I am afraid that the most viable option is to generate a new project with the corresponding MCU and then copy the application source files from your pre-existing project as well as any customizations you made to the project properties.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
      <pubDate>Mon, 23 Sep 2024 19:45:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Compatibility-issue-between-S32K344-and-S32K324/m-p/1960111#M41259</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2024-09-23T19:45:03Z</dc:date>
    </item>
    <item>
      <title>Re: Compatibility issue between S32K344 and S32K324</title>
      <link>https://community.nxp.com/t5/S32K/Compatibility-issue-between-S32K344-and-S32K324/m-p/2295397#M56165</link>
      <description>After the decoupling process, the S32K344 effectively becomes the S32K324. This point has already been clarified in the discussion at &lt;A href="https://community.nxp.com/t5/S32K/How-do-I-configure-SMP-FreeRTOS-on-the-S32K344/m-p/2295127#M56161" target="_blank"&gt;https://community.nxp.com/t5/S32K/How-do-I-configure-SMP-FreeRTOS-on-the-S32K344/m-p/2295127#M56161&lt;/A&gt;, and I would like to verify it with you once more.</description>
      <pubDate>Sat, 17 Jan 2026 11:56:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Compatibility-issue-between-S32K344-and-S32K324/m-p/2295397#M56165</guid>
      <dc:creator>yanyanwang</dc:creator>
      <dc:date>2026-01-17T11:56:42Z</dc:date>
    </item>
  </channel>
</rss>