<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックLIN Communication error s32k142</title>
    <link>https://community.nxp.com/t5/S32K/LIN-Communication-error-s32k142/m-p/1959742#M41239</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hello Team,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;1. I am trying to run 3 way valve but , from code i am getting slave not responding error and&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;at next iteration time getting slave response as shown in LOG file.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2. i have two log files attached ,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;A) One from TLIN PRo software when shedule table is run it runs normally without any errors,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;B) when i am running from software code (Attached LIN zip ) it gives response some times and some times gives error - slave not responding., receive Frames drop inconsistently.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;please verify the LPUART1_IRQ_handler in LIN.c file&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can you please help to feedback on the same.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;1.All Components are giving correct response except response from TWVheatcore (0x33) .&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2.Above LOG from CVTMS TACO software is written for only TWVheatcore (0x32) and reading response (0x33).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3.From TACO Software and running from TLINPro software delay are same as per given in LDF.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;4.Observation : At start 3 way valve is moving from 100% -&amp;gt;127%-&amp;gt;100%-&amp;gt;0% , itakes 15 second's to complete its init sequence After that it follows command inputs given from user.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;5.Is there any special case we need to read for TWVheatcore response(0x33) ? and Delay adjustments?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 23 Sep 2024 09:24:20 GMT</pubDate>
    <dc:creator>bhushangs101</dc:creator>
    <dc:date>2024-09-23T09:24:20Z</dc:date>
    <item>
      <title>LIN Communication error s32k142</title>
      <link>https://community.nxp.com/t5/S32K/LIN-Communication-error-s32k142/m-p/1959742#M41239</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello Team,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;1. I am trying to run 3 way valve but , from code i am getting slave not responding error and&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;at next iteration time getting slave response as shown in LOG file.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2. i have two log files attached ,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;A) One from TLIN PRo software when shedule table is run it runs normally without any errors,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;B) when i am running from software code (Attached LIN zip ) it gives response some times and some times gives error - slave not responding., receive Frames drop inconsistently.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;please verify the LPUART1_IRQ_handler in LIN.c file&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can you please help to feedback on the same.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;1.All Components are giving correct response except response from TWVheatcore (0x33) .&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2.Above LOG from CVTMS TACO software is written for only TWVheatcore (0x32) and reading response (0x33).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3.From TACO Software and running from TLINPro software delay are same as per given in LDF.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;4.Observation : At start 3 way valve is moving from 100% -&amp;gt;127%-&amp;gt;100%-&amp;gt;0% , itakes 15 second's to complete its init sequence After that it follows command inputs given from user.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;5.Is there any special case we need to read for TWVheatcore response(0x33) ? and Delay adjustments?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 23 Sep 2024 09:24:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LIN-Communication-error-s32k142/m-p/1959742#M41239</guid>
      <dc:creator>bhushangs101</dc:creator>
      <dc:date>2024-09-23T09:24:20Z</dc:date>
    </item>
    <item>
      <title>Re: LIN Communication error s32k142</title>
      <link>https://community.nxp.com/t5/S32K/LIN-Communication-error-s32k142/m-p/1962706#M41370</link>
      <description>&lt;P&gt;discussed over individual Case already.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Thu, 26 Sep 2024 13:15:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LIN-Communication-error-s32k142/m-p/1962706#M41370</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-09-26T13:15:04Z</dc:date>
    </item>
  </channel>
</rss>