<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K312 FCCU</title>
    <link>https://community.nxp.com/t5/S32K/S32K312-FCCU/m-p/1959736#M41237</link>
    <description>&lt;P&gt;I would like to know a simple way to configure FCCU on S32K312 to detect (not inject) any RAM or Flash errors and report them. I can read the FCCU registers periodically to check if there are any errors. Is this possible at all?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it possible to configure the FCCU to detect Interrupt line stuck at fault?&lt;/P&gt;</description>
    <pubDate>Mon, 23 Sep 2024 09:17:33 GMT</pubDate>
    <dc:creator>rameshnairmetallic</dc:creator>
    <dc:date>2024-09-23T09:17:33Z</dc:date>
    <item>
      <title>S32K312 FCCU</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-FCCU/m-p/1959736#M41237</link>
      <description>&lt;P&gt;I would like to know a simple way to configure FCCU on S32K312 to detect (not inject) any RAM or Flash errors and report them. I can read the FCCU registers periodically to check if there are any errors. Is this possible at all?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it possible to configure the FCCU to detect Interrupt line stuck at fault?&lt;/P&gt;</description>
      <pubDate>Mon, 23 Sep 2024 09:17:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-FCCU/m-p/1959736#M41237</guid>
      <dc:creator>rameshnairmetallic</dc:creator>
      <dc:date>2024-09-23T09:17:33Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 FCCU</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-FCCU/m-p/1959873#M41247</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;the simplest way is to directly configure FCCU via FCCU registers.&lt;/P&gt;
&lt;P&gt;Once there is any RAM of Flash error reported by memories, it will be latched in FCCU status register.&lt;/P&gt;
&lt;P&gt;Depending on the FCCU configuration you can trigger:&lt;/P&gt;
&lt;P&gt;1. reset&lt;/P&gt;
&lt;P&gt;2. interrupt&lt;/P&gt;
&lt;P&gt;3. no reaction&lt;/P&gt;
&lt;P&gt;If the fault is enabled and the Alarm interrupt it triggered you can read in ISR the root cause of the fault and take appropriate action.&lt;/P&gt;
&lt;P&gt;Basically you don't need any driver as it is simple static configuration of few registers.&lt;/P&gt;
&lt;P&gt;For more details you can refer to functional description chapter in FCCU in reference manual.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Mon, 23 Sep 2024 11:41:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-FCCU/m-p/1959873#M41247</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2024-09-23T11:41:59Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 FCCU</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-FCCU/m-p/1985512#M42766</link>
      <description>&lt;P&gt;DOes the variant S32K312 have the Safety modules mentioned in the manual.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;6.13 Safety related modules..........................................................................................................84&lt;BR /&gt;6.13.1 EIM module............................................................................................................................. 84&lt;BR /&gt;6.13.2 ERM module........................................................................................................................... 84&lt;BR /&gt;6.13.3 CRC module............................................................................................................................85&lt;BR /&gt;6.13.4 FCCU module......................................................................................................................... 85&lt;BR /&gt;6.13.5 STCU2 module........................................................................................................................87&lt;BR /&gt;6.13.6 Temperature sensor ...............................................................................................................88&lt;BR /&gt;6.13.7 Reset and Standby safety measures...................................................................................... 89&lt;BR /&gt;6.13.8 DCF clients..............................................................................................................................89&lt;/P&gt;</description>
      <pubDate>Thu, 31 Oct 2024 11:30:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-FCCU/m-p/1985512#M42766</guid>
      <dc:creator>rameshnairmetallic</dc:creator>
      <dc:date>2024-10-31T11:30:52Z</dc:date>
    </item>
  </channel>
</rss>