<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: S32K344-DCF Example</title>
    <link>https://community.nxp.com/t5/S32K/S32K344-DCF-Example/m-p/1957404#M41116</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;1. yes,&amp;nbsp;&lt;SPAN&gt;just continue writing to the unprogrammed addresses, in your case 0x1B000770.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;2. Parity is in bit 1 of control word as you wrote. The parity scheme used is even parity. So, the number of 1s in the data word and parity field needs to be even. So for data&amp;nbsp;&lt;SPAN&gt;0x00000100, parity should be set and so control word will be&amp;nbsp;0x00100006&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;BR, Petr&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 19 Sep 2024 08:09:20 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2024-09-19T08:09:20Z</dc:date>
    <item>
      <title>S32K344-DCF Example</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-DCF-Example/m-p/1956450#M41052</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;Are there any sample programs or detailed documentation about DCF?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BestRegards,&lt;/P&gt;&lt;P&gt;Simon&lt;/P&gt;</description>
      <pubDate>Wed, 18 Sep 2024 08:32:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-DCF-Example/m-p/1956450#M41052</guid>
      <dc:creator>Simon-Liu</dc:creator>
      <dc:date>2024-09-18T08:32:10Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344-DCF Example</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-DCF-Example/m-p/1956622#M41070</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;for more info refer to&amp;nbsp;Chapter 37 Device Configuration Format (DCF) records&amp;nbsp; and S32K3xx_DCF_clients excel file attached to the device RM.&lt;BR /&gt;You can refer to below example to know how to program DCF record using RTD code;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-decouple-RTD400-Ip-C40-DS35-v1/ta-p/1866329" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-decouple-RTD400-Ip-C40-DS35-v1/ta-p/1866329&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Wed, 18 Sep 2024 11:47:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-DCF-Example/m-p/1956622#M41070</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-09-18T11:47:51Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344-DCF Example</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-DCF-Example/m-p/1957104#M41090</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52961"&gt;@PetrS&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Thank you for your reply I have the following questions about the example &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;1. Why is the Flash address where the dcf_client_utest_misc data is written 0x1B000768? &lt;/SPAN&gt;&lt;SPAN class=""&gt;According to the description of S32K3xx_DCF_clients.xlsx in RM, isn't the starting address of UTEST- DCF Records 0x1B000708? &lt;/SPAN&gt;&lt;SPAN class=""&gt;So what is the write address of other DCF clients? &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;2. As shown in the screenshot below, are the descriptions of DCF Control Word and DCF Data Word reversed? &lt;/SPAN&gt;&lt;SPAN class=""&gt;The value of DCF Control Word should be 0x00100004, right?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="SimonLiu_0-1726714522639.jpeg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/299848iFCDEC7F13F7DCD87/image-size/medium?v=v2&amp;amp;px=400" role="button" title="SimonLiu_0-1726714522639.jpeg" alt="SimonLiu_0-1726714522639.jpeg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;3. If you want to set the Parity and Stop bits, should they be 0x00100006 and 0x00100005 respectively?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;BestRegards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Simon&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 19 Sep 2024 02:56:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-DCF-Example/m-p/1957104#M41090</guid>
      <dc:creator>Simon-Liu</dc:creator>
      <dc:date>2024-09-19T02:56:39Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344-DCF Example</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-DCF-Example/m-p/1957346#M41112</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;1. DCF records are some data in OTP, this is programed only once, not erasable, you can just add new records after the last one. You need to determine the destination program address in UTEST flash. DCF records starts from 0x1B000700. Find out the first double-word filled by 0xFF. This is the target program address: “0x1B000768”&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="PetrS_0-1726730634727.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/299920iF64612C7D4B5095C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="PetrS_0-1726730634727.png" alt="PetrS_0-1726730634727.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;For each new write this address will increase, for sure.&lt;/P&gt;
&lt;P&gt;2. yes, in the example a description is swapped&lt;/P&gt;
&lt;P&gt;3. Parity should be properly calculated and set accordingly, but Stop bit must be always cleared. Otherwise a record will be taken as last one and next one will be ignored.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Thu, 19 Sep 2024 07:32:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-DCF-Example/m-p/1957346#M41112</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-09-19T07:32:51Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344-DCF Example</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-DCF-Example/m-p/1957373#M41114</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52961"&gt;@PetrS&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your answer&lt;BR /&gt;1. In the EVB Flash I use, there is already a record at address 0x1B000768. And this record is for configuring dcf_client_utest_misc.&lt;BR /&gt;If I want to configure dcf_client_utest_misc differently, can I just continue writing to the unprogrammed addresses behind? For example, write 0x00000100 and 0x00100004.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="SimonLiu_0-1726731877659.jpeg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/299933i1AA299E79187C377/image-size/medium?v=v2&amp;amp;px=400" role="button" title="SimonLiu_0-1726731877659.jpeg" alt="SimonLiu_0-1726731877659.jpeg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;3. I would like to ask where the Parity is located, is it bit 1 of DCF Control Word? Because the description of RM confuses me.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="SimonLiu_1-1726731888966.jpeg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/299934iBD4514E7BB1F3691/image-size/medium?v=v2&amp;amp;px=400" role="button" title="SimonLiu_1-1726731888966.jpeg" alt="SimonLiu_1-1726731888966.jpeg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BestRegards,&lt;/P&gt;&lt;P&gt;Simon&lt;/P&gt;</description>
      <pubDate>Thu, 19 Sep 2024 07:45:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-DCF-Example/m-p/1957373#M41114</guid>
      <dc:creator>Simon-Liu</dc:creator>
      <dc:date>2024-09-19T07:45:29Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344-DCF Example</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-DCF-Example/m-p/1957404#M41116</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;1. yes,&amp;nbsp;&lt;SPAN&gt;just continue writing to the unprogrammed addresses, in your case 0x1B000770.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;2. Parity is in bit 1 of control word as you wrote. The parity scheme used is even parity. So, the number of 1s in the data word and parity field needs to be even. So for data&amp;nbsp;&lt;SPAN&gt;0x00000100, parity should be set and so control word will be&amp;nbsp;0x00100006&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;BR, Petr&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 19 Sep 2024 08:09:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-DCF-Example/m-p/1957404#M41116</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-09-19T08:09:20Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344-DCF Example</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-DCF-Example/m-p/1957435#M41122</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52961"&gt;@PetrS&lt;/a&gt;&amp;nbsp;, do you have a description of the default DCF records which are already present in the uC when delivered to TIER1 ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;See attachment , they do not appear in the DCF clients (xls)&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks a lot, Ovidiu&lt;/P&gt;</description>
      <pubDate>Thu, 19 Sep 2024 08:29:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-DCF-Example/m-p/1957435#M41122</guid>
      <dc:creator>ovidiubriscan</dc:creator>
      <dc:date>2024-09-19T08:29:00Z</dc:date>
    </item>
  </channel>
</rss>