<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Exiting Core Standby Mode using WKUP[4] on S32k312 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Exiting-Core-Standby-Mode-using-WKUP-4-on-S32k312/m-p/1955569#M41001</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;I am using the S32k312 board. I am currently able to wakeup the board from STANDBY mode when the GPIO PTA13 is configured as WKUP[4].&amp;nbsp; I am also able to wakeup the board from CORE-STANDBY mode when I configure the same pin as EIRQ[21].&lt;/P&gt;&lt;P&gt;I am not able to wakeup the board from CORE_STANDBY mode using WKUP[4].&amp;nbsp; I want to wake it up using the WKUP[4] as I also using the same pin to wake it up from STANDBY Mode. I have taken care of all the peripherals that have to be kept running while in CORE_STANDBY mode.&lt;/P&gt;&lt;P&gt;Can you please help me with this issue ?&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Saransh Goel&lt;/P&gt;</description>
    <pubDate>Tue, 17 Sep 2024 11:21:48 GMT</pubDate>
    <dc:creator>saranshgoel</dc:creator>
    <dc:date>2024-09-17T11:21:48Z</dc:date>
    <item>
      <title>Exiting Core Standby Mode using WKUP[4] on S32k312</title>
      <link>https://community.nxp.com/t5/S32K/Exiting-Core-Standby-Mode-using-WKUP-4-on-S32k312/m-p/1955569#M41001</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;I am using the S32k312 board. I am currently able to wakeup the board from STANDBY mode when the GPIO PTA13 is configured as WKUP[4].&amp;nbsp; I am also able to wakeup the board from CORE-STANDBY mode when I configure the same pin as EIRQ[21].&lt;/P&gt;&lt;P&gt;I am not able to wakeup the board from CORE_STANDBY mode using WKUP[4].&amp;nbsp; I want to wake it up using the WKUP[4] as I also using the same pin to wake it up from STANDBY Mode. I have taken care of all the peripherals that have to be kept running while in CORE_STANDBY mode.&lt;/P&gt;&lt;P&gt;Can you please help me with this issue ?&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Saransh Goel&lt;/P&gt;</description>
      <pubDate>Tue, 17 Sep 2024 11:21:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Exiting-Core-Standby-Mode-using-WKUP-4-on-S32k312/m-p/1955569#M41001</guid>
      <dc:creator>saranshgoel</dc:creator>
      <dc:date>2024-09-17T11:21:48Z</dc:date>
    </item>
    <item>
      <title>Re: Exiting Core Standby Mode using WKUP[4] on S32k312</title>
      <link>https://community.nxp.com/t5/S32K/Exiting-Core-Standby-Mode-using-WKUP-4-on-S32k312/m-p/1957685#M41142</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/237627"&gt;@saranshgoel&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I have just been testing it, and I see the WPKU interrupt (nofitication) works when the core is in CORE_STANDBY (WFI).&lt;/P&gt;
&lt;P&gt;Please share your project.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Thu, 19 Sep 2024 12:19:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Exiting-Core-Standby-Mode-using-WKUP-4-on-S32k312/m-p/1957685#M41142</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2024-09-19T12:19:00Z</dc:date>
    </item>
    <item>
      <title>Re: Exiting Core Standby Mode using WKUP[4] on S32k312</title>
      <link>https://community.nxp.com/t5/S32K/Exiting-Core-Standby-Mode-using-WKUP-4-on-S32k312/m-p/1960665#M41281</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your reply. I have figured out the issue. There was a mistake in the interrupt configurations. It works on my end too now.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Saransh Goel&lt;/P&gt;</description>
      <pubDate>Tue, 24 Sep 2024 09:31:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Exiting-Core-Standby-Mode-using-WKUP-4-on-S32k312/m-p/1960665#M41281</guid>
      <dc:creator>saranshgoel</dc:creator>
      <dc:date>2024-09-24T09:31:38Z</dc:date>
    </item>
  </channel>
</rss>