<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K1XX FLEXCAN</title>
    <link>https://community.nxp.com/t5/S32K/S32K1XX-FLEXCAN/m-p/1954607#M40947</link>
    <description>&lt;P&gt;hello ,experts:&lt;/P&gt;&lt;P&gt;We know FLEXCAN support CAN receive by MB and RXFIFO&lt;/P&gt;&lt;P&gt;I have a question that when i config Message received in&amp;nbsp;RXFIFO mode with interrupt ,the rxFIFO engine&amp;nbsp;occupied 0-5MB,and i set 8 &amp;nbsp;Rx FIFO Filters which&amp;nbsp;occupied 2MB&amp;nbsp;&lt;/P&gt;&lt;P&gt;so the first 8 MB is used for&amp;nbsp; rxFIFO engine and&amp;nbsp;Filters element. there are 24 MB (S32K116)left,.&lt;/P&gt;&lt;P&gt;It is clear that i can config any MB in the range of left MB for transmit&amp;nbsp; ,BUT I wonder that&amp;nbsp; if i can set a&amp;nbsp;MB used for Receive, Even i have used RX FIFO.&amp;nbsp;&lt;/P&gt;&lt;P&gt;if yes ? can you share a demo for me ?&lt;/P&gt;&lt;P&gt;if no , that means the MB after FIFO could only used for transmit MB ?&lt;/P&gt;</description>
    <pubDate>Sat, 14 Sep 2024 06:56:24 GMT</pubDate>
    <dc:creator>PINKMAN</dc:creator>
    <dc:date>2024-09-14T06:56:24Z</dc:date>
    <item>
      <title>S32K1XX FLEXCAN</title>
      <link>https://community.nxp.com/t5/S32K/S32K1XX-FLEXCAN/m-p/1954607#M40947</link>
      <description>&lt;P&gt;hello ,experts:&lt;/P&gt;&lt;P&gt;We know FLEXCAN support CAN receive by MB and RXFIFO&lt;/P&gt;&lt;P&gt;I have a question that when i config Message received in&amp;nbsp;RXFIFO mode with interrupt ,the rxFIFO engine&amp;nbsp;occupied 0-5MB,and i set 8 &amp;nbsp;Rx FIFO Filters which&amp;nbsp;occupied 2MB&amp;nbsp;&lt;/P&gt;&lt;P&gt;so the first 8 MB is used for&amp;nbsp; rxFIFO engine and&amp;nbsp;Filters element. there are 24 MB (S32K116)left,.&lt;/P&gt;&lt;P&gt;It is clear that i can config any MB in the range of left MB for transmit&amp;nbsp; ,BUT I wonder that&amp;nbsp; if i can set a&amp;nbsp;MB used for Receive, Even i have used RX FIFO.&amp;nbsp;&lt;/P&gt;&lt;P&gt;if yes ? can you share a demo for me ?&lt;/P&gt;&lt;P&gt;if no , that means the MB after FIFO could only used for transmit MB ?&lt;/P&gt;</description>
      <pubDate>Sat, 14 Sep 2024 06:56:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K1XX-FLEXCAN/m-p/1954607#M40947</guid>
      <dc:creator>PINKMAN</dc:creator>
      <dc:date>2024-09-14T06:56:24Z</dc:date>
    </item>
    <item>
      <title>Re: S32K1XX FLEXCAN</title>
      <link>https://community.nxp.com/t5/S32K/S32K1XX-FLEXCAN/m-p/1955070#M40969</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;rest of available MBs can be set for both TX and/or RX operation.&lt;BR /&gt;Some SDK based example is posted at&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-FlexCAN-RXFIFO-DMA-S32DS-ARM-2018-R1/ta-p/1120014" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-FlexCAN-RXFIFO-DMA-S32DS-ARM-2018-R1/ta-p/1120014&lt;/A&gt;&lt;BR /&gt;Hope it helps.&lt;/P&gt;
&lt;P&gt;BR, Petr&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 16 Sep 2024 08:54:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K1XX-FLEXCAN/m-p/1955070#M40969</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-09-16T08:54:47Z</dc:date>
    </item>
    <item>
      <title>Re: S32K1XX FLEXCAN</title>
      <link>https://community.nxp.com/t5/S32K/S32K1XX-FLEXCAN/m-p/1955264#M40982</link>
      <description>&lt;P&gt;thank you ! in fact, if i use RXFIFO meanwhile i also set a MB for RX, if the message passed the filter element ,so the MB for RX will not be used ?&lt;/P&gt;</description>
      <pubDate>Mon, 16 Sep 2024 15:22:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K1XX-FLEXCAN/m-p/1955264#M40982</guid>
      <dc:creator>PINKMAN</dc:creator>
      <dc:date>2024-09-16T15:22:57Z</dc:date>
    </item>
    <item>
      <title>Re: S32K1XX FLEXCAN</title>
      <link>https://community.nxp.com/t5/S32K/S32K1XX-FLEXCAN/m-p/1955465#M40991</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;depends on the setting, but if RXFIFO is set to be searched first and&amp;nbsp;the Rx FIFO is a matched structure and is free-to-receive, then the Rx FIFO is the matching winner regardless of the scan for MBs. Then at the end of matching process the message is moved-in to RXFIFO.&lt;BR /&gt;I can recommend to read chapters Receive Process and Matching Process of the device RM.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Tue, 17 Sep 2024 07:24:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K1XX-FLEXCAN/m-p/1955465#M40991</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-09-17T07:24:30Z</dc:date>
    </item>
    <item>
      <title>Re: S32K1XX FLEXCAN</title>
      <link>https://community.nxp.com/t5/S32K/S32K1XX-FLEXCAN/m-p/1955594#M41005</link>
      <description>&lt;P&gt;非常感谢&lt;/P&gt;</description>
      <pubDate>Tue, 17 Sep 2024 11:56:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K1XX-FLEXCAN/m-p/1955594#M41005</guid>
      <dc:creator>PINKMAN</dc:creator>
      <dc:date>2024-09-17T11:56:30Z</dc:date>
    </item>
    <item>
      <title>Re: S32K1XX FLEXCAN</title>
      <link>https://community.nxp.com/t5/S32K/S32K1XX-FLEXCAN/m-p/1956146#M41029</link>
      <description>&lt;P&gt;i'm sorry, there is still a question that if i use RXFIFO, i can only set mask with FLEXCAN_RX_MASK_INDIVIDUAL ? which means only use&amp;nbsp;RXIMR and RXFGMASK to config filter items and other MBs. uder this condition(use RXFIFO),i think use&amp;nbsp;RXMGMASK, RX14MASK, RX15MASK is a wrong configration maybe?&lt;/P&gt;</description>
      <pubDate>Wed, 18 Sep 2024 02:57:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K1XX-FLEXCAN/m-p/1956146#M41029</guid>
      <dc:creator>PINKMAN</dc:creator>
      <dc:date>2024-09-18T02:57:18Z</dc:date>
    </item>
    <item>
      <title>Re: S32K1XX FLEXCAN</title>
      <link>https://community.nxp.com/t5/S32K/S32K1XX-FLEXCAN/m-p/1956573#M41063</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;up to 32 elements of the filter table are individually affected by the Individual Mask&lt;BR /&gt;Registers (RXIMRx), according to the setting of CTRL2[RFFN], if individual mask scheme is used (IMRQ=1). If the IRMQ bit is negated, then the FIFO filter table is affected by RXFGMASK only and&amp;nbsp;&lt;SPAN&gt;RXMGMASK, RX14MASK, RX15MASK are used for rest of MBs.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR, Petr&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 18 Sep 2024 10:36:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K1XX-FLEXCAN/m-p/1956573#M41063</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-09-18T10:36:04Z</dc:date>
    </item>
    <item>
      <title>Re: S32K1XX FLEXCAN</title>
      <link>https://community.nxp.com/t5/S32K/S32K1XX-FLEXCAN/m-p/1956670#M41072</link>
      <description>&lt;P&gt;OK ,I GOT IT.NB! THANKS&lt;/P&gt;</description>
      <pubDate>Wed, 18 Sep 2024 13:01:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K1XX-FLEXCAN/m-p/1956670#M41072</guid>
      <dc:creator>PINKMAN</dc:creator>
      <dc:date>2024-09-18T13:01:51Z</dc:date>
    </item>
  </channel>
</rss>