<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32k344 microcontroller GPIO configuration</title>
    <link>https://community.nxp.com/t5/S32K/S32k344-microcontroller-GPIO-configuration/m-p/1953297#M40884</link>
    <description>&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;i am using s32designstudio for coding and i have configured some GPIO pin with help of autoupdate code, but in autoupadte code only macro is genarated for pin and port.&lt;BR /&gt;&lt;BR /&gt;so i want to set,reset that pin from application layer ,there is any function to call from application layer ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Thu, 12 Sep 2024 08:49:51 GMT</pubDate>
    <dc:creator>Omkar9903</dc:creator>
    <dc:date>2024-09-12T08:49:51Z</dc:date>
    <item>
      <title>S32k344 microcontroller GPIO configuration</title>
      <link>https://community.nxp.com/t5/S32K/S32k344-microcontroller-GPIO-configuration/m-p/1953297#M40884</link>
      <description>&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;i am using s32designstudio for coding and i have configured some GPIO pin with help of autoupdate code, but in autoupadte code only macro is genarated for pin and port.&lt;BR /&gt;&lt;BR /&gt;so i want to set,reset that pin from application layer ,there is any function to call from application layer ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Thu, 12 Sep 2024 08:49:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k344-microcontroller-GPIO-configuration/m-p/1953297#M40884</guid>
      <dc:creator>Omkar9903</dc:creator>
      <dc:date>2024-09-12T08:49:51Z</dc:date>
    </item>
    <item>
      <title>Re: S32k344 microcontroller GPIO configuration</title>
      <link>https://community.nxp.com/t5/S32K/S32k344-microcontroller-GPIO-configuration/m-p/1954424#M40942</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/238723"&gt;@Omkar9903&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;You can refer to the Siul2_Port_Ip_Example_S32K344, which configures the red LED, and calls the&amp;nbsp;Siul2_Dio_Ip_WritePin() function. You can also refer to all of the functions in the Siul2_Dio_Ip.c file.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
      <pubDate>Fri, 13 Sep 2024 17:41:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k344-microcontroller-GPIO-configuration/m-p/1954424#M40942</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-09-13T17:41:02Z</dc:date>
    </item>
  </channel>
</rss>