<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32Kのトピックs32k3 read DFLASH failed</title>
    <link>https://community.nxp.com/t5/S32K/s32k3-read-DFLASH-failed/m-p/1953223#M40878</link>
    <description>&lt;P&gt;&lt;FONT&gt;Hello, I tried to use Mem_43_InFls module in S32K311, I write test code to test the api of the module , and find that I can write and erase the DFLASH(0X10000000-0X1000FFFF) successfully, but when I try to read the data in DFLASH(such as the data in 0X10000000), the program will shut down.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ZMY666777_0-1726126803281.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/298790iAB00B995A84E120A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ZMY666777_0-1726126803281.png" alt="ZMY666777_0-1726126803281.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ZMY666777_0-1726126803281.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;test code are shown above. I first use write api and can successfully write dflash. and I set readflag to 1 manually. And will fail to read dflash. after debug, I find the program will shut down when run '&lt;SPAN&gt;(*((uint8 *)(0x10000000)))'. I can read other address such as PFLASH. So I wonder what kind of reason will cause this problem.&lt;BR /&gt;Thanks!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 12 Sep 2024 07:44:26 GMT</pubDate>
    <dc:creator>ZMY666777</dc:creator>
    <dc:date>2024-09-12T07:44:26Z</dc:date>
    <item>
      <title>s32k3 read DFLASH failed</title>
      <link>https://community.nxp.com/t5/S32K/s32k3-read-DFLASH-failed/m-p/1953223#M40878</link>
      <description>&lt;P&gt;&lt;FONT&gt;Hello, I tried to use Mem_43_InFls module in S32K311, I write test code to test the api of the module , and find that I can write and erase the DFLASH(0X10000000-0X1000FFFF) successfully, but when I try to read the data in DFLASH(such as the data in 0X10000000), the program will shut down.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ZMY666777_0-1726126803281.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/298790iAB00B995A84E120A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ZMY666777_0-1726126803281.png" alt="ZMY666777_0-1726126803281.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ZMY666777_0-1726126803281.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;test code are shown above. I first use write api and can successfully write dflash. and I set readflag to 1 manually. And will fail to read dflash. after debug, I find the program will shut down when run '&lt;SPAN&gt;(*((uint8 *)(0x10000000)))'. I can read other address such as PFLASH. So I wonder what kind of reason will cause this problem.&lt;BR /&gt;Thanks!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 12 Sep 2024 07:44:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k3-read-DFLASH-failed/m-p/1953223#M40878</guid>
      <dc:creator>ZMY666777</dc:creator>
      <dc:date>2024-09-12T07:44:26Z</dc:date>
    </item>
    <item>
      <title>Re: s32k3 read DFLASH failed</title>
      <link>https://community.nxp.com/t5/S32K/s32k3-read-DFLASH-failed/m-p/1953413#M40893</link>
      <description>&lt;P&gt;The problem is solved. The reason is that in my program the dflash is been protected by MPU. after disabling MPU the dflash can be read.&lt;/P&gt;</description>
      <pubDate>Thu, 12 Sep 2024 11:00:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k3-read-DFLASH-failed/m-p/1953413#M40893</guid>
      <dc:creator>ZMY666777</dc:creator>
      <dc:date>2024-09-12T11:00:53Z</dc:date>
    </item>
  </channel>
</rss>