<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32Kのトピックs32k312 flash</title>
    <link>https://community.nxp.com/t5/S32K/s32k312-flash/m-p/1951884#M40827</link>
    <description>&lt;P&gt;Hello, I'm currently using the mem_43_INFLS driver to operate the flash on the s32k312. I have a few points I'd like to consult about:&lt;/P&gt;&lt;P&gt;1. Can I use this driver to erase the pflash under boot mode so that I can update the app program?&lt;/P&gt;&lt;P&gt;2. Can I use this driver to operate the Dflash to simulate EEPROM? If so, are there any corresponding example routines for reference? Thank you!&lt;/P&gt;</description>
    <pubDate>Wed, 11 Sep 2024 08:37:36 GMT</pubDate>
    <dc:creator>fengba_360</dc:creator>
    <dc:date>2024-09-11T08:37:36Z</dc:date>
    <item>
      <title>s32k312 flash</title>
      <link>https://community.nxp.com/t5/S32K/s32k312-flash/m-p/1951884#M40827</link>
      <description>&lt;P&gt;Hello, I'm currently using the mem_43_INFLS driver to operate the flash on the s32k312. I have a few points I'd like to consult about:&lt;/P&gt;&lt;P&gt;1. Can I use this driver to erase the pflash under boot mode so that I can update the app program?&lt;/P&gt;&lt;P&gt;2. Can I use this driver to operate the Dflash to simulate EEPROM? If so, are there any corresponding example routines for reference? Thank you!&lt;/P&gt;</description>
      <pubDate>Wed, 11 Sep 2024 08:37:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k312-flash/m-p/1951884#M40827</guid>
      <dc:creator>fengba_360</dc:creator>
      <dc:date>2024-09-11T08:37:36Z</dc:date>
    </item>
    <item>
      <title>Re: s32k312 flash</title>
      <link>https://community.nxp.com/t5/S32K/s32k312-flash/m-p/1953216#M40877</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/238047"&gt;@fengba_360&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;1. Yes&lt;/P&gt;
&lt;P&gt;2. For the SW emulated EEPROM, there is the RTD FEE driver.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1726126306161.png" style="width: 650px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/298785i320E264B05D95180/image-dimensions/650x382?v=v2" width="650" height="382" role="button" title="danielmartynek_0-1726126306161.png" alt="danielmartynek_0-1726126306161.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielmartynek_0-1726126306161.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Thu, 12 Sep 2024 07:33:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k312-flash/m-p/1953216#M40877</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2024-09-12T07:33:31Z</dc:date>
    </item>
    <item>
      <title>Re: s32k312 flash</title>
      <link>https://community.nxp.com/t5/S32K/s32k312-flash/m-p/1953368#M40889</link>
      <description>What's the difference between FEE and Mem_43_INFLS? I'm quite confused. Could you please guide me further? I have two requirements: one is to erase and write app programs during boot, and the other is to simulate EEPROM under the app.</description>
      <pubDate>Thu, 12 Sep 2024 09:51:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k312-flash/m-p/1953368#M40889</guid>
      <dc:creator>fengba_360</dc:creator>
      <dc:date>2024-09-12T09:51:02Z</dc:date>
    </item>
    <item>
      <title>Re: s32k312 flash</title>
      <link>https://community.nxp.com/t5/S32K/s32k312-flash/m-p/1953407#M40891</link>
      <description>&lt;P&gt;As I said, FLS is for programming / erasing the flash, FEE is used to emulate the EEPROM.&lt;/P&gt;
&lt;P&gt;Refer to the User Manual and Integration Manual of the drivers that can be found in the installation directory of the RTD.&lt;/P&gt;
&lt;P&gt;Or have a look at Autosar documentation:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.autosar.org/fileadmin/standards/R22-11/CP/AUTOSAR_SWS_FlashEEPROMEmulation.pdf" target="_blank"&gt;https://www.autosar.org/fileadmin/standards/R22-11/CP/AUTOSAR_SWS_FlashEEPROMEmulation.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Thu, 12 Sep 2024 10:50:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k312-flash/m-p/1953407#M40891</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2024-09-12T10:50:01Z</dc:date>
    </item>
  </channel>
</rss>