<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: No BTCU_FIFO2_REQUEST DMAMUX SOURCE ?</title>
    <link>https://community.nxp.com/t5/S32K/No-BTCU-FIFO2-REQUEST-DMAMUX-SOURCE/m-p/1949748#M40684</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;this chip has two instances of DMAMUX: DMAMUX_0 and DMAMUX_1. See the DMAMUX map file attached to device RM to find information about DMA requests assignment.&amp;nbsp;&lt;BR /&gt;&lt;SPAN&gt;BTCU_FIFO2_REQUEST is routed to DMAMUX_1&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="PetrS_0-1725861947371.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/297807i9E183301B4181747/image-size/medium?v=v2&amp;amp;px=400" role="button" title="PetrS_0-1725861947371.png" alt="PetrS_0-1725861947371.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;PetrS_0-1725861947371.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Mon, 09 Sep 2024 06:08:14 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2024-09-09T06:08:14Z</dc:date>
    <item>
      <title>No BTCU_FIFO2_REQUEST DMAMUX SOURCE ?</title>
      <link>https://community.nxp.com/t5/S32K/No-BTCU-FIFO2-REQUEST-DMAMUX-SOURCE/m-p/1949329#M40652</link>
      <description>&lt;P&gt;I can't see a dmamux source for bctu fifo2.&lt;BR /&gt;&lt;BR /&gt;does it not exist? don't see that being mentioned anywhere in the data sheet.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot 2024-09-06 at 2.04.36 PM.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/297685i58253DD57B9DEBA3/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot 2024-09-06 at 2.04.36 PM.png" alt="Screenshot 2024-09-06 at 2.04.36 PM.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Screenshot 2024-09-06 at 2.04.36 PM.png&lt;/span&gt;&lt;/span&gt;&lt;BR /&gt;&lt;BR /&gt;i have two separate hw triggers for the bctu to start two separate conversion lists and store the results in a fifo and have a dma to move them over and then trigger the callback in the dma completion to use the adc data.&amp;nbsp;&lt;BR /&gt;but cannot do this for the second fifo seemingly as there is not a source for the dma mux to do this with.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 06 Sep 2024 21:08:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/No-BTCU-FIFO2-REQUEST-DMAMUX-SOURCE/m-p/1949329#M40652</guid>
      <dc:creator>not_a_duck</dc:creator>
      <dc:date>2024-09-06T21:08:31Z</dc:date>
    </item>
    <item>
      <title>Re: No BTCU_FIFO2_REQUEST DMAMUX SOURCE ?</title>
      <link>https://community.nxp.com/t5/S32K/No-BTCU-FIFO2-REQUEST-DMAMUX-SOURCE/m-p/1949748#M40684</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;this chip has two instances of DMAMUX: DMAMUX_0 and DMAMUX_1. See the DMAMUX map file attached to device RM to find information about DMA requests assignment.&amp;nbsp;&lt;BR /&gt;&lt;SPAN&gt;BTCU_FIFO2_REQUEST is routed to DMAMUX_1&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="PetrS_0-1725861947371.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/297807i9E183301B4181747/image-size/medium?v=v2&amp;amp;px=400" role="button" title="PetrS_0-1725861947371.png" alt="PetrS_0-1725861947371.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;PetrS_0-1725861947371.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Mon, 09 Sep 2024 06:08:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/No-BTCU-FIFO2-REQUEST-DMAMUX-SOURCE/m-p/1949748#M40684</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-09-09T06:08:14Z</dc:date>
    </item>
    <item>
      <title>Re: No BTCU_FIFO2_REQUEST DMAMUX SOURCE ?</title>
      <link>https://community.nxp.com/t5/S32K/No-BTCU-FIFO2-REQUEST-DMAMUX-SOURCE/m-p/1950330#M40730</link>
      <description>&lt;P&gt;Thanks! that was the issue. had to use a dma channel that used dmamux 1. used channel 17 in this case and now it works!&lt;/P&gt;</description>
      <pubDate>Mon, 09 Sep 2024 20:18:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/No-BTCU-FIFO2-REQUEST-DMAMUX-SOURCE/m-p/1950330#M40730</guid>
      <dc:creator>not_a_duck</dc:creator>
      <dc:date>2024-09-09T20:18:37Z</dc:date>
    </item>
  </channel>
</rss>