<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32Kのトピックuint32 startup getAipsRegisterValue(void) and uint32 startup_getControlRegisterValue(void)</title>
    <link>https://community.nxp.com/t5/S32K/uint32-startup-getAipsRegisterValue-void-and-uint32-startup/m-p/1948991#M40638</link>
    <description>&lt;P&gt;Where is the definition of startup_getAipsRegisterValue() and startup_getControlRegisterValue()？&lt;/P&gt;&lt;P&gt;When I enabled the MCAL_ENABLE_USER_MODE_SUPPORT definition in the S32K344 code, the compiler reported an error that it could not find the definitions for both functions.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="NaYil_0-1725618744997.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/297577iD828D2D73B3F6054/image-size/medium?v=v2&amp;amp;px=400" alt="NaYil_0-1725618744997.png" title="NaYil_0-1725618744997.png" /&gt;&lt;/span&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;With best wishes&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 06 Sep 2024 10:37:21 GMT</pubDate>
    <dc:creator>NaYil</dc:creator>
    <dc:date>2024-09-06T10:37:21Z</dc:date>
    <item>
      <title>uint32 startup getAipsRegisterValue(void) and uint32 startup_getControlRegisterValue(void)</title>
      <link>https://community.nxp.com/t5/S32K/uint32-startup-getAipsRegisterValue-void-and-uint32-startup/m-p/1948991#M40638</link>
      <description>&lt;P&gt;Where is the definition of startup_getAipsRegisterValue() and startup_getControlRegisterValue()？&lt;/P&gt;&lt;P&gt;When I enabled the MCAL_ENABLE_USER_MODE_SUPPORT definition in the S32K344 code, the compiler reported an error that it could not find the definitions for both functions.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="NaYil_0-1725618744997.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/297577iD828D2D73B3F6054/image-size/medium?v=v2&amp;amp;px=400" alt="NaYil_0-1725618744997.png" title="NaYil_0-1725618744997.png" /&gt;&lt;/span&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;With best wishes&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 06 Sep 2024 10:37:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/uint32-startup-getAipsRegisterValue-void-and-uint32-startup/m-p/1948991#M40638</guid>
      <dc:creator>NaYil</dc:creator>
      <dc:date>2024-09-06T10:37:21Z</dc:date>
    </item>
    <item>
      <title>Re: uint32 startup getAipsRegisterValue(void) and uint32 startup_getControlRegisterValue(void)</title>
      <link>https://community.nxp.com/t5/S32K/uint32-startup-getAipsRegisterValue-void-and-uint32-startup/m-p/1951399#M40798</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/239286"&gt;@NaYil&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Sorry for the delay.&amp;nbsp;Due to workload, my response might be delayed.&lt;/P&gt;
&lt;P&gt;The MCAL_ENABLE_USER_MODE_SUPPORT macro must be added to the project properties under C/C++ Build &amp;gt; Settings &amp;gt; Standard S32DS C Compiler &amp;gt; Preprocessor and Standard S32DS Assembler &amp;gt; Preprocessor.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Let me know if this works for you.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
      <pubDate>Tue, 10 Sep 2024 19:20:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/uint32-startup-getAipsRegisterValue-void-and-uint32-startup/m-p/1951399#M40798</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2024-09-10T19:20:30Z</dc:date>
    </item>
  </channel>
</rss>