<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: strange Signal at ADC input</title>
    <link>https://community.nxp.com/t5/S32K/strange-Signal-at-ADC-input/m-p/880745#M4057</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;Could you please send the schematic and describe the ADC operation in more details?&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;BR, Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 Mar 2019 15:15:02 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2019-03-25T15:15:02Z</dc:date>
    <item>
      <title>strange Signal at ADC input</title>
      <link>https://community.nxp.com/t5/S32K/strange-Signal-at-ADC-input/m-p/880744#M4056</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see a strange signal at ADC input which might cause the issue I am faced with.&lt;/P&gt;&lt;P&gt;I have attached the osci picture.&lt;/P&gt;&lt;P&gt;This signal looks like a sawtooth wave.&lt;/P&gt;&lt;P&gt;When I change the paramter SMPLTS then the area marked on the picture changes accordingly.&lt;/P&gt;&lt;P&gt;So I assume that when the ADC does "sample" the signal is forced to input level.&lt;/P&gt;&lt;P&gt;When the ADC does "hold" for internal sampling the signal follows a sawtooth wave.&lt;/P&gt;&lt;P&gt;I do not see this signal analysing the sample values. However the sampled signal does not match what I expect. Also I have&lt;/P&gt;&lt;P&gt;issue processing it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The ADC input in connected with 1nF capacitor to ground.&lt;/P&gt;&lt;P&gt;Does anybody has n idea why this signal is so strange? What do I need to do here?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Mar 2019 16:00:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/strange-Signal-at-ADC-input/m-p/880744#M4056</guid>
      <dc:creator>edgarmichel</dc:creator>
      <dc:date>2019-03-22T16:00:36Z</dc:date>
    </item>
    <item>
      <title>Re: strange Signal at ADC input</title>
      <link>https://community.nxp.com/t5/S32K/strange-Signal-at-ADC-input/m-p/880745#M4057</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;Could you please send the schematic and describe the ADC operation in more details?&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;BR, Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Mar 2019 15:15:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/strange-Signal-at-ADC-input/m-p/880745#M4057</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2019-03-25T15:15:02Z</dc:date>
    </item>
    <item>
      <title>Re: strange Signal at ADC input</title>
      <link>https://community.nxp.com/t5/S32K/strange-Signal-at-ADC-input/m-p/880746#M4058</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Daniel,&lt;BR /&gt;I found an Application Note&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN4373.pdf" title="https://www.nxp.com/docs/en/application-note/AN4373.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN4373.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It seems that is the root cause ie the input impadance does not match.&lt;BR /&gt;I will check that&lt;/P&gt;&lt;P&gt;BR Edgar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Mar 2019 19:56:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/strange-Signal-at-ADC-input/m-p/880746#M4058</guid>
      <dc:creator>edgarmichel</dc:creator>
      <dc:date>2019-03-25T19:56:04Z</dc:date>
    </item>
  </channel>
</rss>