<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32M244LC high-voltage detect threshold</title>
    <link>https://community.nxp.com/t5/S32K/S32M244LC-high-voltage-detect-threshold/m-p/1946192#M40486</link>
    <description>&lt;P&gt;Hi Yan,&lt;/P&gt;
&lt;P&gt;there is a possibility to set bit&amp;nbsp;HDHVDCFG to 1 , in GDU/CFG register (S32M24x RM rev2, page 1165).&amp;nbsp; With this bit set, thresholds VHVHDHA and VHVHDHD will be used for overvoltage detector. Thresholds VHVHDHA (min-typ-max: 30.65-32.5-34.6V) and VHVHDHD (min-typ-max: 29.65-31.5-33.6V) are defined in S32M2xx DS rev3, page 38/39&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Pavel&lt;/P&gt;</description>
    <pubDate>Tue, 03 Sep 2024 10:24:16 GMT</pubDate>
    <dc:creator>PavelL</dc:creator>
    <dc:date>2024-09-03T10:24:16Z</dc:date>
    <item>
      <title>S32M244LC high-voltage detect threshold</title>
      <link>https://community.nxp.com/t5/S32K/S32M244LC-high-voltage-detect-threshold/m-p/1945802#M40466</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;I have a question about high voltage threshold Settings，S32M244LC‘s GDU will be closed when VSUP over 22.6V，Where can I set this value(such as set to 28V)，No description of this section is found in the RM &amp;amp;datasheet.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Sep 2024 02:47:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32M244LC-high-voltage-detect-threshold/m-p/1945802#M40466</guid>
      <dc:creator>YAN3</dc:creator>
      <dc:date>2024-09-03T02:47:47Z</dc:date>
    </item>
    <item>
      <title>Re: S32M244LC high-voltage detect threshold</title>
      <link>https://community.nxp.com/t5/S32K/S32M244LC-high-voltage-detect-threshold/m-p/1946192#M40486</link>
      <description>&lt;P&gt;Hi Yan,&lt;/P&gt;
&lt;P&gt;there is a possibility to set bit&amp;nbsp;HDHVDCFG to 1 , in GDU/CFG register (S32M24x RM rev2, page 1165).&amp;nbsp; With this bit set, thresholds VHVHDHA and VHVHDHD will be used for overvoltage detector. Thresholds VHVHDHA (min-typ-max: 30.65-32.5-34.6V) and VHVHDHD (min-typ-max: 29.65-31.5-33.6V) are defined in S32M2xx DS rev3, page 38/39&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Tue, 03 Sep 2024 10:24:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32M244LC-high-voltage-detect-threshold/m-p/1946192#M40486</guid>
      <dc:creator>PavelL</dc:creator>
      <dc:date>2024-09-03T10:24:16Z</dc:date>
    </item>
    <item>
      <title>Re: S32M244LC high-voltage detect threshold</title>
      <link>https://community.nxp.com/t5/S32K/S32M244LC-high-voltage-detect-threshold/m-p/1946718#M40516</link>
      <description>&lt;P&gt;hi&amp;nbsp;&lt;SPAN&gt;Pavel，&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp;&lt;/SPAN&gt;Thank you and regards,&lt;/P&gt;</description>
      <pubDate>Wed, 04 Sep 2024 00:38:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32M244LC-high-voltage-detect-threshold/m-p/1946718#M40516</guid>
      <dc:creator>YAN3</dc:creator>
      <dc:date>2024-09-04T00:38:22Z</dc:date>
    </item>
  </channel>
</rss>