<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Issues with working UART communication in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Issues-with-working-UART-communication/m-p/1944044#M40361</link>
    <description>&lt;P&gt;Hi&amp;nbsp;Santhosh,&lt;/P&gt;
&lt;P class="lia-align-left"&gt;1. Are you using S32K116EVB2Q048 or S32K116EVB-Q048?&lt;BR /&gt;2. J107 is used to select whether to be powered by P5V_SDA_PSW (J7 USB) or P5V_SBC (J16 external 12v). How do you set J107?&lt;BR /&gt;3. Which signal is the logic analyzer connected to? Is the GND signal connected?&lt;BR /&gt;4. Please show me the signal observed by the oscilloscope&lt;BR /&gt;5. Have you tested the UART project in S32K1 SDK or RTD?&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Fri, 30 Aug 2024 04:10:08 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2024-08-30T04:10:08Z</dc:date>
    <item>
      <title>Issues with working UART communication</title>
      <link>https://community.nxp.com/t5/S32K/Issues-with-working-UART-communication/m-p/1943307#M40290</link>
      <description>&lt;P&gt;Hello all,&lt;BR /&gt;&lt;SPAN&gt;I'm working on lpUART with S32K116 EVB, everything is working as expected if I power up the device from USB port. However, if I try to provide power supply from external Power Adapter 12V I could see unsual behaviour or unwanted signals coming from UART peripheral on logic analyzer as shown in below figure.&amp;nbsp;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="santhosh23_0-1724922119153.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/296029i9CDB2A483F97BAD7/image-size/medium?v=v2&amp;amp;px=400" role="button" title="santhosh23_0-1724922119153.png" alt="santhosh23_0-1724922119153.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;santhosh23_0-1724922119153.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Is there anything that we have to consider if we are providing external 12 V supply?&lt;BR /&gt;&lt;BR /&gt;Thanks in advance!&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Santhosh&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Aug 2024 09:04:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Issues-with-working-UART-communication/m-p/1943307#M40290</guid>
      <dc:creator>santhosh23</dc:creator>
      <dc:date>2024-08-29T09:04:58Z</dc:date>
    </item>
    <item>
      <title>Re: Issues with working UART communication</title>
      <link>https://community.nxp.com/t5/S32K/Issues-with-working-UART-communication/m-p/1944044#M40361</link>
      <description>&lt;P&gt;Hi&amp;nbsp;Santhosh,&lt;/P&gt;
&lt;P class="lia-align-left"&gt;1. Are you using S32K116EVB2Q048 or S32K116EVB-Q048?&lt;BR /&gt;2. J107 is used to select whether to be powered by P5V_SDA_PSW (J7 USB) or P5V_SBC (J16 external 12v). How do you set J107?&lt;BR /&gt;3. Which signal is the logic analyzer connected to? Is the GND signal connected?&lt;BR /&gt;4. Please show me the signal observed by the oscilloscope&lt;BR /&gt;5. Have you tested the UART project in S32K1 SDK or RTD?&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 30 Aug 2024 04:10:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Issues-with-working-UART-communication/m-p/1944044#M40361</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-08-30T04:10:08Z</dc:date>
    </item>
  </channel>
</rss>