<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic CAN-FD clocked by FIRC in S32K</title>
    <link>https://community.nxp.com/t5/S32K/CAN-FD-clocked-by-FIRC/m-p/879378#M4033</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&amp;nbsp;&lt;/P&gt;&lt;P&gt;According to &lt;A href="https://www.can-cia.org/fileadmin/resources/documents/proceedings/2013_mutter.pdf"&gt;this document&amp;nbsp;&lt;/A&gt;(Robustness of a CAN FD Bus System) with a clock of 40MHz the oscillator tolerance range accepted in CAN FD for bitrates from 500Kb/s up to 10Mb/s is in the range 0/0.75%.&lt;/P&gt;&lt;P&gt;Furthermore, to achieve standard baud rates normally an external oscillator of 40MHz is required.&amp;nbsp;&lt;/P&gt;&lt;P&gt;My question is:&amp;nbsp;&lt;/P&gt;&lt;P&gt;The CAN peripheral on the S32K1xx MCUs is meant to be used in conjunction with an external oscillator or with an internal oscillator?&lt;BR /&gt;FIRC oscillator has a worst case tolerance in the range of the 1% (up to 1.1 above 125degrees).&lt;/P&gt;&lt;P&gt;In K116 the FIRC is the main clock source, the implication here is that is not possible to use the MCU and CAN peripheral for high baud rates without external oscillator - or am I wrong?&lt;/P&gt;&lt;P&gt;Is there some reference or application note from NXP that relates CAN baud rates and oscillator/internal clock requirements?&lt;/P&gt;&lt;P&gt;Any hint in general?&lt;/P&gt;&lt;P&gt;Kind Regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;L.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;P.S.&lt;/P&gt;&lt;P&gt;Please note that uisng two EVB we were able to run correctly CAN-FD examples. Then the validation with other commercial tools has some troubles, hence my question about FIRC and ext osc.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 01 Feb 2019 08:34:00 GMT</pubDate>
    <dc:creator>Catosh</dc:creator>
    <dc:date>2019-02-01T08:34:00Z</dc:date>
    <item>
      <title>CAN-FD clocked by FIRC</title>
      <link>https://community.nxp.com/t5/S32K/CAN-FD-clocked-by-FIRC/m-p/879378#M4033</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&amp;nbsp;&lt;/P&gt;&lt;P&gt;According to &lt;A href="https://www.can-cia.org/fileadmin/resources/documents/proceedings/2013_mutter.pdf"&gt;this document&amp;nbsp;&lt;/A&gt;(Robustness of a CAN FD Bus System) with a clock of 40MHz the oscillator tolerance range accepted in CAN FD for bitrates from 500Kb/s up to 10Mb/s is in the range 0/0.75%.&lt;/P&gt;&lt;P&gt;Furthermore, to achieve standard baud rates normally an external oscillator of 40MHz is required.&amp;nbsp;&lt;/P&gt;&lt;P&gt;My question is:&amp;nbsp;&lt;/P&gt;&lt;P&gt;The CAN peripheral on the S32K1xx MCUs is meant to be used in conjunction with an external oscillator or with an internal oscillator?&lt;BR /&gt;FIRC oscillator has a worst case tolerance in the range of the 1% (up to 1.1 above 125degrees).&lt;/P&gt;&lt;P&gt;In K116 the FIRC is the main clock source, the implication here is that is not possible to use the MCU and CAN peripheral for high baud rates without external oscillator - or am I wrong?&lt;/P&gt;&lt;P&gt;Is there some reference or application note from NXP that relates CAN baud rates and oscillator/internal clock requirements?&lt;/P&gt;&lt;P&gt;Any hint in general?&lt;/P&gt;&lt;P&gt;Kind Regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;L.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;P.S.&lt;/P&gt;&lt;P&gt;Please note that uisng two EVB we were able to run correctly CAN-FD examples. Then the validation with other commercial tools has some troubles, hence my question about FIRC and ext osc.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Feb 2019 08:34:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-FD-clocked-by-FIRC/m-p/879378#M4033</guid>
      <dc:creator>Catosh</dc:creator>
      <dc:date>2019-02-01T08:34:00Z</dc:date>
    </item>
    <item>
      <title>Re: CAN-FD clocked by FIRC</title>
      <link>https://community.nxp.com/t5/S32K/CAN-FD-clocked-by-FIRC/m-p/879379#M4034</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;You can refer to &lt;A href="https://www.nxp.com/docs/en/application-note/AN1798.pdf"&gt;AN1798 CAN Bit Timing Requirements&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;It depends on the system and configuration.&lt;/P&gt;&lt;P&gt;If higher tolerace is required than the FIRC specification, you should use SOSC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Feb 2019 14:17:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-FD-clocked-by-FIRC/m-p/879379#M4034</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2019-02-05T14:17:11Z</dc:date>
    </item>
    <item>
      <title>Re: CAN-FD clocked by FIRC</title>
      <link>https://community.nxp.com/t5/S32K/CAN-FD-clocked-by-FIRC/m-p/1567772#M19372</link>
      <description>&lt;P&gt;Hello，&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;If the oscillator is used as the clock source, what frequency of oscillator is required for the baud rate of CAN FD 500Kbps/2Mbps, and is frequency 8Mhz of oscillator OK?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 11 Dec 2022 12:56:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-FD-clocked-by-FIRC/m-p/1567772#M19372</guid>
      <dc:creator>ben_chin</dc:creator>
      <dc:date>2022-12-11T12:56:34Z</dc:date>
    </item>
  </channel>
</rss>