<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: NXP S32k312 debugger connection issue after adding Image Vector  Table Marker</title>
    <link>https://community.nxp.com/t5/S32K/NXP-S32k312-debugger-connection-issue-after-adding-Image-Vector/m-p/1941909#M40207</link>
    <description>&lt;P&gt;Hi Dexter,&lt;/P&gt;
&lt;P&gt;The SBAF searches for a valid IVT at these addresses only:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1724831210980.png" style="width: 641px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/295719iD03D6C66C1CA5756/image-dimensions/641x234?v=v2" width="641" height="234" role="button" title="danielmartynek_0-1724831210980.png" alt="danielmartynek_0-1724831210980.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;What debugger do you use?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 28 Aug 2024 07:47:14 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2024-08-28T07:47:14Z</dc:date>
    <item>
      <title>NXP S32k312 debugger connection issue after adding Image Vector  Table Marker</title>
      <link>https://community.nxp.com/t5/S32K/NXP-S32k312-debugger-connection-issue-after-adding-Image-Vector/m-p/1941153#M40165</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using S32k312 (100 pin)which is working perfect with debugger. I need to add Image&amp;nbsp;Vector Table at location 0x400000 for working without debugger. When I add this change, software run fine without debugger but when connected back to debugger, breakpoints are not hitting in initial code start areas like startup code, main function etc (program continuously running).&lt;BR /&gt;&lt;BR /&gt;What will be the reason for this?&lt;BR /&gt;&lt;BR /&gt;Thanks and regards&lt;BR /&gt;Dexter.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 27 Aug 2024 09:24:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/NXP-S32k312-debugger-connection-issue-after-adding-Image-Vector/m-p/1941153#M40165</guid>
      <dc:creator>dextervictoria</dc:creator>
      <dc:date>2024-08-27T09:24:36Z</dc:date>
    </item>
    <item>
      <title>Re: NXP S32k312 debugger connection issue after adding Image Vector  Table Marker</title>
      <link>https://community.nxp.com/t5/S32K/NXP-S32k312-debugger-connection-issue-after-adding-Image-Vector/m-p/1941909#M40207</link>
      <description>&lt;P&gt;Hi Dexter,&lt;/P&gt;
&lt;P&gt;The SBAF searches for a valid IVT at these addresses only:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1724831210980.png" style="width: 641px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/295719iD03D6C66C1CA5756/image-dimensions/641x234?v=v2" width="641" height="234" role="button" title="danielmartynek_0-1724831210980.png" alt="danielmartynek_0-1724831210980.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;What debugger do you use?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 28 Aug 2024 07:47:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/NXP-S32k312-debugger-connection-issue-after-adding-Image-Vector/m-p/1941909#M40207</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2024-08-28T07:47:14Z</dc:date>
    </item>
    <item>
      <title>Re: NXP S32k312 debugger connection issue after adding Image Vector  Table Marker</title>
      <link>https://community.nxp.com/t5/S32K/NXP-S32k312-debugger-connection-issue-after-adding-Image-Vector/m-p/1943092#M40271</link>
      <description>&lt;P&gt;Hi Daniel,&lt;BR /&gt;I placed IVT at 0x400000 address. I'm using isystem debugger. Also tested in Lauterbach; shows same behaviour.&lt;BR /&gt;Breakpoints at initial functions like boardstart, main, other init functions are not recognised. But break points are recognised from cyclic os tasks.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Dexter.&lt;/P&gt;</description>
      <pubDate>Thu, 29 Aug 2024 06:18:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/NXP-S32k312-debugger-connection-issue-after-adding-Image-Vector/m-p/1943092#M40271</guid>
      <dc:creator>dextervictoria</dc:creator>
      <dc:date>2024-08-29T06:18:17Z</dc:date>
    </item>
    <item>
      <title>Re: NXP S32k312 debugger connection issue after adding Image Vector  Table Marker</title>
      <link>https://community.nxp.com/t5/S32K/NXP-S32k312-debugger-connection-issue-after-adding-Image-Vector/m-p/1944473#M40407</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/239653"&gt;@dextervictoria&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I understand you are attaching the debugger while the MCU is already running, that mean after the startup code.&lt;/P&gt;
&lt;P&gt;With Lauterbach, you can use a script like this:&lt;/P&gt;
&lt;P&gt;SYStem.CPU S32K312&lt;BR /&gt;wait state.power()&lt;BR /&gt;SYStem.Mode Attach&lt;BR /&gt;Break&lt;/P&gt;
&lt;P&gt;This should wait while the MCU is not powered, and attach/break once the MCU is powered.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 30 Aug 2024 12:10:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/NXP-S32k312-debugger-connection-issue-after-adding-Image-Vector/m-p/1944473#M40407</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2024-08-30T12:10:58Z</dc:date>
    </item>
  </channel>
</rss>