<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックADC 2 instance for s32k344</title>
    <link>https://community.nxp.com/t5/S32K/ADC-2-instance-for-s32k344/m-p/1938453#M39998</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am triggering&amp;nbsp; the ADC at&amp;nbsp; each reload event of a pwm signal through the BCTU , the issue i am facing is that when i am triggering the ADC instance 2 at 40 kHz is working i can sample the data from the input , but when i am trying to sampling it at 2kHz there are no input , i do not have that issue at ADC 1 AND 2&amp;nbsp;instance, what do i miss here ?&lt;/P&gt;&lt;P&gt;i am using S32k344 .RTD 3.00&lt;/P&gt;</description>
    <pubDate>Thu, 22 Aug 2024 12:10:53 GMT</pubDate>
    <dc:creator>Ayaz</dc:creator>
    <dc:date>2024-08-22T12:10:53Z</dc:date>
    <item>
      <title>ADC 2 instance for s32k344</title>
      <link>https://community.nxp.com/t5/S32K/ADC-2-instance-for-s32k344/m-p/1938453#M39998</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am triggering&amp;nbsp; the ADC at&amp;nbsp; each reload event of a pwm signal through the BCTU , the issue i am facing is that when i am triggering the ADC instance 2 at 40 kHz is working i can sample the data from the input , but when i am trying to sampling it at 2kHz there are no input , i do not have that issue at ADC 1 AND 2&amp;nbsp;instance, what do i miss here ?&lt;/P&gt;&lt;P&gt;i am using S32k344 .RTD 3.00&lt;/P&gt;</description>
      <pubDate>Thu, 22 Aug 2024 12:10:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ADC-2-instance-for-s32k344/m-p/1938453#M39998</guid>
      <dc:creator>Ayaz</dc:creator>
      <dc:date>2024-08-22T12:10:53Z</dc:date>
    </item>
    <item>
      <title>Re: ADC 2 instance for s32k344</title>
      <link>https://community.nxp.com/t5/S32K/ADC-2-instance-for-s32k344/m-p/1938794#M40024</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@Ayaz" target="_blank"&gt;Hi@Ayaz&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I can't give you a suitable solution from your description.&lt;/P&gt;
&lt;P&gt;You need to provide a demo that can reproduce the problem so that we can help you&lt;/P&gt;
&lt;P&gt;troubleshoot the cause of the problem.&lt;/P&gt;</description>
      <pubDate>Fri, 23 Aug 2024 01:43:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ADC-2-instance-for-s32k344/m-p/1938794#M40024</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2024-08-23T01:43:43Z</dc:date>
    </item>
  </channel>
</rss>