<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic DMA configuration in S32K</title>
    <link>https://community.nxp.com/t5/S32K/DMA-configuration/m-p/1933622#M39603</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using s32k96 UC &amp;amp; configured of dmaLogicChannel_Type_0 with CH16 using DMA_IP_HW_INST_1 interrupt.&lt;/P&gt;&lt;P&gt;I have attached the one image I want to change the ISR time but not getting which parameter is configure for ISR time.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;BR Omkar.&lt;/P&gt;</description>
    <pubDate>Fri, 16 Aug 2024 10:36:27 GMT</pubDate>
    <dc:creator>Omkar9903</dc:creator>
    <dc:date>2024-08-16T10:36:27Z</dc:date>
    <item>
      <title>DMA configuration</title>
      <link>https://community.nxp.com/t5/S32K/DMA-configuration/m-p/1933622#M39603</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using s32k96 UC &amp;amp; configured of dmaLogicChannel_Type_0 with CH16 using DMA_IP_HW_INST_1 interrupt.&lt;/P&gt;&lt;P&gt;I have attached the one image I want to change the ISR time but not getting which parameter is configure for ISR time.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;BR Omkar.&lt;/P&gt;</description>
      <pubDate>Fri, 16 Aug 2024 10:36:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/DMA-configuration/m-p/1933622#M39603</guid>
      <dc:creator>Omkar9903</dc:creator>
      <dc:date>2024-08-16T10:36:27Z</dc:date>
    </item>
    <item>
      <title>Re: DMA configuration</title>
      <link>https://community.nxp.com/t5/S32K/DMA-configuration/m-p/1935621#M39822</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/238723"&gt;@Omkar9903&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;It is not possible to control the timing of the DMA ISR by simply setting a parameter. However, you can generate a periodic DMA trigger event using the PIT or when a transmit buffer becomes empty or a receive buffer becomes full, periodically. Refer to section 13.4.2.1 (Enable a source with periodic triggering) of the&amp;nbsp;S32K39 and S32K37 Reference Manual, Rev. 3.&lt;/P&gt;
&lt;P&gt;Could you provide more details on the implementation you are looking for?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
      <pubDate>Mon, 19 Aug 2024 21:37:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/DMA-configuration/m-p/1935621#M39822</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2024-08-19T21:37:54Z</dc:date>
    </item>
  </channel>
</rss>