<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic s32k388 eMcem module in Safety Package in S32K</title>
    <link>https://community.nxp.com/t5/S32K/s32k388-eMcem-module-in-Safety-Package/m-p/1932890#M39549</link>
    <description>&lt;P&gt;I see unexpected behavior After initializing eMcem and receiving E_ok from the function "eMcem_Init(&amp;amp;eMcem_Config_0);" ,and enabling the reaction type to "short-reset-reaction" in the configurator for NCF_0 , NCF_2 and NCF_3 causes the software to stop at the vector catch.&lt;/P&gt;</description>
    <pubDate>Thu, 15 Aug 2024 10:23:04 GMT</pubDate>
    <dc:creator>mariam</dc:creator>
    <dc:date>2024-08-15T10:23:04Z</dc:date>
    <item>
      <title>s32k388 eMcem module in Safety Package</title>
      <link>https://community.nxp.com/t5/S32K/s32k388-eMcem-module-in-Safety-Package/m-p/1932890#M39549</link>
      <description>&lt;P&gt;I see unexpected behavior After initializing eMcem and receiving E_ok from the function "eMcem_Init(&amp;amp;eMcem_Config_0);" ,and enabling the reaction type to "short-reset-reaction" in the configurator for NCF_0 , NCF_2 and NCF_3 causes the software to stop at the vector catch.&lt;/P&gt;</description>
      <pubDate>Thu, 15 Aug 2024 10:23:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k388-eMcem-module-in-Safety-Package/m-p/1932890#M39549</guid>
      <dc:creator>mariam</dc:creator>
      <dc:date>2024-08-15T10:23:04Z</dc:date>
    </item>
  </channel>
</rss>