<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Copy code from Flash to RAM and run s32K342</title>
    <link>https://community.nxp.com/t5/S32K/Copy-code-from-Flash-to-RAM-and-run-s32K342/m-p/1931969#M39507</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52613"&gt;@davidtosenovjan&lt;/a&gt;&amp;nbsp; / NXP team,&lt;/P&gt;&lt;P&gt;any update on this topic !&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; regards.&lt;/P&gt;</description>
    <pubDate>Wed, 14 Aug 2024 11:15:58 GMT</pubDate>
    <dc:creator>Kazarian</dc:creator>
    <dc:date>2024-08-14T11:15:58Z</dc:date>
    <item>
      <title>Copy code from Flash to RAM and run s32K342</title>
      <link>https://community.nxp.com/t5/S32K/Copy-code-from-Flash-to-RAM-and-run-s32K342/m-p/1926347#M39012</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am currently working with the S32K342 microcontroller and S32DS v3.5 , SDK v4.0.0, and I have a requirement that during startup the complete program should be copied from flash to RAM . so it will execute fully from RAM.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Probably i need to modify some sections on linker script, also modify the startup code, but im not very familair with this device yet. I would appreciate guidance on how to do it.&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Tue, 06 Aug 2024 11:59:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Copy-code-from-Flash-to-RAM-and-run-s32K342/m-p/1926347#M39012</guid>
      <dc:creator>Kazarian</dc:creator>
      <dc:date>2024-08-06T11:59:43Z</dc:date>
    </item>
    <item>
      <title>Re: Copy code from Flash to RAM and run s32K342</title>
      <link>https://community.nxp.com/t5/S32K/Copy-code-from-Flash-to-RAM-and-run-s32K342/m-p/1929075#M39176</link>
      <description>&lt;P&gt;Here you may find a procedure how to do it:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Run-a-routine-from-RAM-in-S32-Design-Studio/ta-p/1113336" target="_blank"&gt;https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Run-a-routine-from-RAM-in-S32-Design-Studio/ta-p/1113336&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 09 Aug 2024 10:58:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Copy-code-from-Flash-to-RAM-and-run-s32K342/m-p/1929075#M39176</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2024-08-09T10:58:51Z</dc:date>
    </item>
    <item>
      <title>Re: Copy code from Flash to RAM and run s32K342</title>
      <link>https://community.nxp.com/t5/S32K/Copy-code-from-Flash-to-RAM-and-run-s32K342/m-p/1929104#M39181</link>
      <description>&lt;P&gt;Hello David,&lt;/P&gt;&lt;P&gt;this is not what im searching for. the example you provided is just for copying 1 function from flash to RAM.&lt;/P&gt;&lt;P&gt;what i want is to copy the complete code during startup from flash and execute it from RAM only.&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Fri, 09 Aug 2024 12:23:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Copy-code-from-Flash-to-RAM-and-run-s32K342/m-p/1929104#M39181</guid>
      <dc:creator>Kazarian</dc:creator>
      <dc:date>2024-08-09T12:23:34Z</dc:date>
    </item>
    <item>
      <title>Re: Copy code from Flash to RAM and run s32K342</title>
      <link>https://community.nxp.com/t5/S32K/Copy-code-from-Flash-to-RAM-and-run-s32K342/m-p/1931969#M39507</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52613"&gt;@davidtosenovjan&lt;/a&gt;&amp;nbsp; / NXP team,&lt;/P&gt;&lt;P&gt;any update on this topic !&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; regards.&lt;/P&gt;</description>
      <pubDate>Wed, 14 Aug 2024 11:15:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Copy-code-from-Flash-to-RAM-and-run-s32K342/m-p/1931969#M39507</guid>
      <dc:creator>Kazarian</dc:creator>
      <dc:date>2024-08-14T11:15:58Z</dc:date>
    </item>
  </channel>
</rss>