<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic s32k312 flash in S32K</title>
    <link>https://community.nxp.com/t5/S32K/s32k312-flash/m-p/1929650#M39246</link>
    <description>&lt;P&gt;Hello, I used to work with the s32k144 which had a function similar to an analog EEPROM that allowed me to store some calibration data. However, I haven't found a similar feature in the s32k312 that I'm currently working with. Could you please provide some guidance or example code related to this? Thank you.&lt;/P&gt;</description>
    <pubDate>Sun, 11 Aug 2024 03:59:50 GMT</pubDate>
    <dc:creator>fengba_360</dc:creator>
    <dc:date>2024-08-11T03:59:50Z</dc:date>
    <item>
      <title>s32k312 flash</title>
      <link>https://community.nxp.com/t5/S32K/s32k312-flash/m-p/1929650#M39246</link>
      <description>&lt;P&gt;Hello, I used to work with the s32k144 which had a function similar to an analog EEPROM that allowed me to store some calibration data. However, I haven't found a similar feature in the s32k312 that I'm currently working with. Could you please provide some guidance or example code related to this? Thank you.&lt;/P&gt;</description>
      <pubDate>Sun, 11 Aug 2024 03:59:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k312-flash/m-p/1929650#M39246</guid>
      <dc:creator>fengba_360</dc:creator>
      <dc:date>2024-08-11T03:59:50Z</dc:date>
    </item>
    <item>
      <title>Re: s32k312 flash</title>
      <link>https://community.nxp.com/t5/S32K/s32k312-flash/m-p/1930863#M39399</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;See previous discussion:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/EEPROM-Emulation-on-S32K12-Controller/td-p/1766152" target="_self"&gt;EEPROM Emulation on S32K12 Controller&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 13 Aug 2024 07:03:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k312-flash/m-p/1930863#M39399</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-08-13T07:03:34Z</dc:date>
    </item>
  </channel>
</rss>