<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Chip Erase in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Chip-Erase/m-p/1928336#M39115</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have an S32K116 microcontroller, and I flashed code starting from address 0x00 using J-Link. Now, I am unable to flash the microcontroller again.&lt;/P&gt;&lt;P&gt;I can connect to the microcontroller with J-Link and read the memory addresses, but I cannot write to them. I am unable to flash code or perform a chip erase. Is there any chance to recover these boards?&lt;/P&gt;</description>
    <pubDate>Thu, 08 Aug 2024 14:39:38 GMT</pubDate>
    <dc:creator>buccno</dc:creator>
    <dc:date>2024-08-08T14:39:38Z</dc:date>
    <item>
      <title>Chip Erase</title>
      <link>https://community.nxp.com/t5/S32K/Chip-Erase/m-p/1928336#M39115</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have an S32K116 microcontroller, and I flashed code starting from address 0x00 using J-Link. Now, I am unable to flash the microcontroller again.&lt;/P&gt;&lt;P&gt;I can connect to the microcontroller with J-Link and read the memory addresses, but I cannot write to them. I am unable to flash code or perform a chip erase. Is there any chance to recover these boards?&lt;/P&gt;</description>
      <pubDate>Thu, 08 Aug 2024 14:39:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Chip-Erase/m-p/1928336#M39115</guid>
      <dc:creator>buccno</dc:creator>
      <dc:date>2024-08-08T14:39:38Z</dc:date>
    </item>
    <item>
      <title>Re: Chip Erase</title>
      <link>https://community.nxp.com/t5/S32K/Chip-Erase/m-p/1929088#M39180</link>
      <description>&lt;P&gt;I write some redundant data to flash configuration field and then MCU is not working.&lt;/P&gt;</description>
      <pubDate>Fri, 09 Aug 2024 11:36:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Chip-Erase/m-p/1929088#M39180</guid>
      <dc:creator>buccno</dc:creator>
      <dc:date>2024-08-09T11:36:27Z</dc:date>
    </item>
  </channel>
</rss>