<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Power supply from eva board</title>
    <link>https://community.nxp.com/t5/S32K/Power-supply-from-eva-board/m-p/640263#M389</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you so much.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 17 Feb 2017 07:27:06 GMT</pubDate>
    <dc:creator>pietroserao</dc:creator>
    <dc:date>2017-02-17T07:27:06Z</dc:date>
    <item>
      <title>Power supply from eva board</title>
      <link>https://community.nxp.com/t5/S32K/Power-supply-from-eva-board/m-p/640261#M387</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good morning i have some questions.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using a FRDMPK 144-Q100 S32k144 Evaluation board.&lt;/P&gt;&lt;P&gt;1) Can this microcontroller works with a 3.3V supply voltage?&lt;/P&gt;&lt;P&gt;2) Can i set the 3,3 V VDD voltage only using the evaluation board, without using external power supply?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;There is some setup?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Feb 2017 08:45:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Power-supply-from-eva-board/m-p/640261#M387</guid>
      <dc:creator>pietroserao</dc:creator>
      <dc:date>2017-02-16T08:45:11Z</dc:date>
    </item>
    <item>
      <title>Re: Power supply from eva board</title>
      <link>https://community.nxp.com/t5/S32K/Power-supply-from-eva-board/m-p/640262#M388</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Pietro,&lt;/P&gt;&lt;P&gt;Yes this MCU can operate down to 2.7V&lt;/P&gt;&lt;P&gt;There is an unpopulated jumper at J10 which can allow to select between 3.3V and 5.0V. You'll need to remove the R64 which is a zero-ohm jumper that directly connects 5.0V to the micro - this needs to be removed so you can make a selection for 3.3V&lt;/P&gt;&lt;P&gt;Schematic attached.&lt;/P&gt;&lt;P&gt;#schematic&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Feb 2017 19:21:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Power-supply-from-eva-board/m-p/640262#M388</guid>
      <dc:creator>allen_willson</dc:creator>
      <dc:date>2017-02-16T19:21:26Z</dc:date>
    </item>
    <item>
      <title>Re: Power supply from eva board</title>
      <link>https://community.nxp.com/t5/S32K/Power-supply-from-eva-board/m-p/640263#M389</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you so much.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Feb 2017 07:27:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Power-supply-from-eva-board/m-p/640263#M389</guid>
      <dc:creator>pietroserao</dc:creator>
      <dc:date>2017-02-17T07:27:06Z</dc:date>
    </item>
  </channel>
</rss>