<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K312 MBIST LBIST in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K312-MBIST-LBIST/m-p/1921292#M38566</link>
    <description>&lt;P&gt;Can you please provide some sample code.&lt;/P&gt;</description>
    <pubDate>Wed, 31 Jul 2024 07:03:37 GMT</pubDate>
    <dc:creator>rameshnairmetallic</dc:creator>
    <dc:date>2024-07-31T07:03:37Z</dc:date>
    <item>
      <title>S32K312 MBIST LBIST</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-MBIST-LBIST/m-p/1920573#M38510</link>
      <description>&lt;P&gt;How can i configure MBIST and LBIST to run on wakeup in S32K312? Is it possible.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How can I configure LBIST to detect interrupt line stuck at faults?&lt;/P&gt;</description>
      <pubDate>Tue, 30 Jul 2024 13:50:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-MBIST-LBIST/m-p/1920573#M38510</guid>
      <dc:creator>rameshnairmetallic</dc:creator>
      <dc:date>2024-07-30T13:50:22Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 MBIST LBIST</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-MBIST-LBIST/m-p/1920813#M38541</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/237886"&gt;@rameshnairmetallic&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The S32K3 devices supports only Online BIST (started by application, not by Bootrom). It is purely on customer app when to execute the Online BIST, execution of the BIST should have same results either if executed in startup phase or in shutdown phase, therefore no effect to FMEDA.&lt;/P&gt;
&lt;P&gt;What need to be considered are prerequisites before executing the BIST as described in the BIST UM chapter: Self-Test prerequisites.&lt;/P&gt;
&lt;P&gt;The supported BIST detailed programming sequence for supported configurations are available&amp;nbsp;in the BIST UM.&amp;nbsp;Also there are available the API to configure and run the LBIST/MBIST tests, the API to read results of the LBIST/MBIST tests, the APIs to monitor status of the LBIST/MBIST tests and Result analysis of the LBIST/MBIST execution initiated by itself.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
      <pubDate>Tue, 30 Jul 2024 18:10:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-MBIST-LBIST/m-p/1920813#M38541</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2024-07-30T18:10:20Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 MBIST LBIST</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-MBIST-LBIST/m-p/1921292#M38566</link>
      <description>&lt;P&gt;Can you please provide some sample code.&lt;/P&gt;</description>
      <pubDate>Wed, 31 Jul 2024 07:03:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-MBIST-LBIST/m-p/1921292#M38566</guid>
      <dc:creator>rameshnairmetallic</dc:creator>
      <dc:date>2024-07-31T07:03:37Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 MBIST LBIST</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-MBIST-LBIST/m-p/1922078#M38613</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/237886"&gt;@rameshnairmetallic&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;A BIST example code is included in the S32_SPD_Demo,&amp;nbsp;which is provided with the&amp;nbsp;S32K3 Safety Peripheral Drivers (&lt;A href="https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-STDSW-D" target="_blank" rel="noopener"&gt;SW32K3-STDSW-D&lt;/A&gt;&amp;nbsp;&amp;gt; Automotive SW - S32K3 - Safety Peripheral Drivers (SPD)).&lt;/P&gt;</description>
      <pubDate>Wed, 31 Jul 2024 20:15:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-MBIST-LBIST/m-p/1922078#M38613</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2024-07-31T20:15:47Z</dc:date>
    </item>
  </channel>
</rss>