<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: s32k314 jtag debug question</title>
    <link>https://community.nxp.com/t5/S32K/s32k314-jtag-debug-question/m-p/1916720#M38207</link>
    <description>&lt;P&gt;I see what you mean. Thank you for letting me know. I found out for the first time.&lt;/P&gt;</description>
    <pubDate>Thu, 25 Jul 2024 01:40:15 GMT</pubDate>
    <dc:creator>Oido</dc:creator>
    <dc:date>2024-07-25T01:40:15Z</dc:date>
    <item>
      <title>s32k314 jtag debug question</title>
      <link>https://community.nxp.com/t5/S32K/s32k314-jtag-debug-question/m-p/1910202#M37773</link>
      <description>&lt;P&gt;Hello, I built a PCB with s32k314. I'm using JTAG, but I got a problem with 1.5V on the TMS pin and couldn't get into the DEBUG.&lt;BR /&gt;I brought the JTAG circuit of the EVB board of S32K344.&lt;BR /&gt;Isn't it normal for the TMS pin to float 5V with PULL UP?&lt;BR /&gt;The TMS pin is connected to the PTA4 of the MCU through the 5V supply line and not to the other pins.&lt;/P&gt;&lt;P&gt;5V turns to 1.5V after R28 only, so I'm baffled. Is it correct that I have to be HIGH on the TMS to enter debug mode?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="KakaoTalk_20240717_115606949.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/288857i62518BBDA7DF6010/image-size/large?v=v2&amp;amp;px=999" alt="KakaoTalk_20240717_115606949.jpg" title="KakaoTalk_20240717_115606949.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jul 2024 03:02:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k314-jtag-debug-question/m-p/1910202#M37773</guid>
      <dc:creator>Oido</dc:creator>
      <dc:date>2024-07-17T03:02:53Z</dc:date>
    </item>
    <item>
      <title>Re: s32k314 jtag debug question</title>
      <link>https://community.nxp.com/t5/S32K/s32k314-jtag-debug-question/m-p/1914785#M38054</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/226367"&gt;@Oido&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;there must be something wrong, you shouldn't see such voltage on TMS.&lt;/P&gt;
&lt;P&gt;Default function on PTA4 is TMS which is input internally pulled up. Isn't there some shortcut on the board?&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Tue, 23 Jul 2024 07:52:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k314-jtag-debug-question/m-p/1914785#M38054</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2024-07-23T07:52:36Z</dc:date>
    </item>
    <item>
      <title>Re: s32k314 jtag debug question</title>
      <link>https://community.nxp.com/t5/S32K/s32k314-jtag-debug-question/m-p/1915869#M38145</link>
      <description>&lt;P&gt;Hello, I found the right answer.&lt;BR /&gt;The inner pins of the MCU were not soldered.&lt;BR /&gt;The problem was that the company that manufactured the PCB did not check it properly.&lt;BR /&gt;Thank you.&lt;BR /&gt;I'm facing another problem now, can you help me answer other questions?&lt;/P&gt;</description>
      <pubDate>Wed, 24 Jul 2024 06:47:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k314-jtag-debug-question/m-p/1915869#M38145</guid>
      <dc:creator>Oido</dc:creator>
      <dc:date>2024-07-24T06:47:55Z</dc:date>
    </item>
    <item>
      <title>Re: s32k314 jtag debug question</title>
      <link>https://community.nxp.com/t5/S32K/s32k314-jtag-debug-question/m-p/1916083#M38162</link>
      <description>&lt;P&gt;For other questions, please create new thread. There's unwritten rule - one thread, one topic. Then it's easier for us and for customers to search in the history.&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Wed, 24 Jul 2024 10:52:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k314-jtag-debug-question/m-p/1916083#M38162</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2024-07-24T10:52:18Z</dc:date>
    </item>
    <item>
      <title>Re: s32k314 jtag debug question</title>
      <link>https://community.nxp.com/t5/S32K/s32k314-jtag-debug-question/m-p/1916720#M38207</link>
      <description>&lt;P&gt;I see what you mean. Thank you for letting me know. I found out for the first time.&lt;/P&gt;</description>
      <pubDate>Thu, 25 Jul 2024 01:40:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k314-jtag-debug-question/m-p/1916720#M38207</guid>
      <dc:creator>Oido</dc:creator>
      <dc:date>2024-07-25T01:40:15Z</dc:date>
    </item>
  </channel>
</rss>