<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32k118evb heating in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32k118evb-heating/m-p/1916105#M38164</link>
    <description>&lt;P&gt;Dear all&lt;/P&gt;&lt;P&gt;I am facing issue is that S32k118evb is heating too much on mcu part and UJA1169 IC ,red led is continously on and I am unable to flash source code. Earlier it is used to heat little bit whenever I connect 12 volt supply for SPI testing and&amp;nbsp; with 5volt board never get heated, but now with both (supply voltage 12 and 5 volt board is heating too much and unable to flash ).&lt;/P&gt;&lt;P&gt;How can I fix and check cause of issue.&lt;/P&gt;&lt;P&gt;B.R&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ashish&lt;/P&gt;</description>
    <pubDate>Wed, 24 Jul 2024 11:36:03 GMT</pubDate>
    <dc:creator>Ashish4525</dc:creator>
    <dc:date>2024-07-24T11:36:03Z</dc:date>
    <item>
      <title>S32k118evb heating</title>
      <link>https://community.nxp.com/t5/S32K/S32k118evb-heating/m-p/1916105#M38164</link>
      <description>&lt;P&gt;Dear all&lt;/P&gt;&lt;P&gt;I am facing issue is that S32k118evb is heating too much on mcu part and UJA1169 IC ,red led is continously on and I am unable to flash source code. Earlier it is used to heat little bit whenever I connect 12 volt supply for SPI testing and&amp;nbsp; with 5volt board never get heated, but now with both (supply voltage 12 and 5 volt board is heating too much and unable to flash ).&lt;/P&gt;&lt;P&gt;How can I fix and check cause of issue.&lt;/P&gt;&lt;P&gt;B.R&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ashish&lt;/P&gt;</description>
      <pubDate>Wed, 24 Jul 2024 11:36:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k118evb-heating/m-p/1916105#M38164</guid>
      <dc:creator>Ashish4525</dc:creator>
      <dc:date>2024-07-24T11:36:03Z</dc:date>
    </item>
    <item>
      <title>Re: S32k118evb heating</title>
      <link>https://community.nxp.com/t5/S32K/S32k118evb-heating/m-p/1917149#M38223</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/225256"&gt;@Ashish4525&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;the board is obviously somehow damaged, I don't think we can help here.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Thu, 25 Jul 2024 11:31:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k118evb-heating/m-p/1917149#M38223</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2024-07-25T11:31:10Z</dc:date>
    </item>
  </channel>
</rss>