<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32k344 Baud Rate Issue in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32k344-Baud-Rate-Issue/m-p/1915954#M38151</link>
    <description>&lt;P&gt;Did you use TTL-USB serial module to connect UART signals of S32K3 to PC? Have you used an oscilloscope or logic analyzer to measure the serial port signals sent from the PC and the signals sent from the S32K3, such as baud rate and &lt;SPAN&gt;size of the data frame\parity\Stop bits&lt;/SPAN&gt;?&lt;/P&gt;
&lt;P&gt;The information you provided is too little, so I can't help you find the cause of the problem quickly. Would you mind sending me the test project?&lt;/P&gt;</description>
    <pubDate>Wed, 24 Jul 2024 08:30:57 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2024-07-24T08:30:57Z</dc:date>
    <item>
      <title>S32k344 Baud Rate Issue</title>
      <link>https://community.nxp.com/t5/S32K/S32k344-Baud-Rate-Issue/m-p/1910584#M37787</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;I am using Nxp S32k344 board in my project . In this&amp;nbsp; sending data through UART using 115200 Baud rate is working fine but in receiving the data is corrupted in&amp;nbsp; the buffer. I am trying to receive "12345678" but i am receiving some garbage characters as provided in the below attachments.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Note:&amp;nbsp;&lt;/STRONG&gt;I am using LPUART &lt;STRONG&gt;instance 8&lt;/STRONG&gt;&amp;nbsp;with clock frequency 80MHZ&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jul 2024 13:01:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k344-Baud-Rate-Issue/m-p/1910584#M37787</guid>
      <dc:creator>Vamsi421</dc:creator>
      <dc:date>2024-07-17T13:01:30Z</dc:date>
    </item>
    <item>
      <title>Re: S32k344 Baud Rate Issue</title>
      <link>https://community.nxp.com/t5/S32K/S32k344-Baud-Rate-Issue/m-p/1911775#M37834</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Please tell me the S32K3 RTD version, development board model, AUTOSAR MCAL or non-AUTOSAR. Otherwise, I can only suggest you refer to the LPUART routine in S32K3 RTD.&lt;BR /&gt;If you use DMA, it is recommended to refer to &lt;A href="https://community.nxp.com/t5/S32K/The-S32K344-Lpuart-transfer-cannot-receive-data-correctly-when/td-p/1856599" target="_self"&gt;The S32K344 Lpuart transfer cannot receive data correctly when DMA enable&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 19 Jul 2024 02:57:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k344-Baud-Rate-Issue/m-p/1911775#M37834</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-07-19T02:57:35Z</dc:date>
    </item>
    <item>
      <title>Re: S32k344 Baud Rate Issue</title>
      <link>https://community.nxp.com/t5/S32K/S32k344-Baud-Rate-Issue/m-p/1914087#M38005</link>
      <description>Hi,&lt;BR /&gt;Autosar Version : 4.7.0&lt;BR /&gt;* Autosar Revision : ASR_REL_4_7_REV_0000&lt;BR /&gt;* Autosar Conf.Variant :&lt;BR /&gt;* SW Version : 3.0.0&lt;BR /&gt;* Build Version : S32K3_RTD_3_0_0_D2303_ASR_REL_4_7_REV_0000_20230331&lt;BR /&gt;* Development board model:S32K344HMS&lt;BR /&gt;</description>
      <pubDate>Mon, 22 Jul 2024 11:59:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k344-Baud-Rate-Issue/m-p/1914087#M38005</guid>
      <dc:creator>Vamsi421</dc:creator>
      <dc:date>2024-07-22T11:59:22Z</dc:date>
    </item>
    <item>
      <title>Re: S32k344 Baud Rate Issue</title>
      <link>https://community.nxp.com/t5/S32K/S32k344-Baud-Rate-Issue/m-p/1914527#M38031</link>
      <description>&lt;P&gt;Sorry, I don't know which development board you mean by S32K344HMS. Please send me the link. If it is convenient, please upload a simple test project. Otherwise, it is difficult to find the cause quickly with so little information.&lt;/P&gt;</description>
      <pubDate>Tue, 23 Jul 2024 02:00:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k344-Baud-Rate-Issue/m-p/1914527#M38031</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-07-23T02:00:27Z</dc:date>
    </item>
    <item>
      <title>Re: S32k344 Baud Rate Issue</title>
      <link>https://community.nxp.com/t5/S32K/S32k344-Baud-Rate-Issue/m-p/1915102#M38073</link>
      <description>&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/automotive-development-platforms/s32k-mcu-platforms/s32k3x4evb-t172-evaluation-board-for-automotive-general-purpose:S32K3X4EVB-T172" target="_blank"&gt;https://www.nxp.com/design/design-center/development-boards-and-designs/automotive-development-platforms/s32k-mcu-platforms/s32k3x4evb-t172-evaluation-board-for-automotive-general-purpose:S32K3X4EVB-T172&lt;/A&gt;</description>
      <pubDate>Tue, 23 Jul 2024 12:55:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k344-Baud-Rate-Issue/m-p/1915102#M38073</guid>
      <dc:creator>Vamsi421</dc:creator>
      <dc:date>2024-07-23T12:55:31Z</dc:date>
    </item>
    <item>
      <title>Re: S32k344 Baud Rate Issue</title>
      <link>https://community.nxp.com/t5/S32K/S32k344-Baud-Rate-Issue/m-p/1915954#M38151</link>
      <description>&lt;P&gt;Did you use TTL-USB serial module to connect UART signals of S32K3 to PC? Have you used an oscilloscope or logic analyzer to measure the serial port signals sent from the PC and the signals sent from the S32K3, such as baud rate and &lt;SPAN&gt;size of the data frame\parity\Stop bits&lt;/SPAN&gt;?&lt;/P&gt;
&lt;P&gt;The information you provided is too little, so I can't help you find the cause of the problem quickly. Would you mind sending me the test project?&lt;/P&gt;</description>
      <pubDate>Wed, 24 Jul 2024 08:30:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k344-Baud-Rate-Issue/m-p/1915954#M38151</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-07-24T08:30:57Z</dc:date>
    </item>
    <item>
      <title>Re: S32k344 Baud Rate Issue</title>
      <link>https://community.nxp.com/t5/S32K/S32k344-Baud-Rate-Issue/m-p/1916100#M38163</link>
      <description>send me the test project with 115200 baudrate&lt;BR /&gt;</description>
      <pubDate>Wed, 24 Jul 2024 11:27:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k344-Baud-Rate-Issue/m-p/1916100#M38163</guid>
      <dc:creator>Vamsi421</dc:creator>
      <dc:date>2024-07-24T11:27:32Z</dc:date>
    </item>
    <item>
      <title>Re: S32k344 Baud Rate Issue</title>
      <link>https://community.nxp.com/t5/S32K/S32k344-Baud-Rate-Issue/m-p/1916830#M38213</link>
      <description>&lt;P&gt;Please test the example &lt;A href="https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/S32K/34863/1/K344_UART_DMA_Working.zip" target="_self"&gt;&lt;STRONG&gt;K344_UART_DMA_Working.zip&lt;/STRONG&gt;&lt;/A&gt;&amp;nbsp;(&lt;SPAN&gt;S32K3_RTD_3_0_0_D2303&lt;/SPAN&gt;) that I gave you in the web link to ensure that your TTL-USB serial module and PC host computer are working properly.&lt;BR /&gt;PTA29(lpuart2_tx) and PTA30(lpuart2_rx)&lt;BR /&gt;9600 baudrate&lt;BR /&gt;If it can be received correctly, then only a slight modification is needed.&lt;/P&gt;</description>
      <pubDate>Thu, 25 Jul 2024 05:06:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k344-Baud-Rate-Issue/m-p/1916830#M38213</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-07-25T05:06:09Z</dc:date>
    </item>
  </channel>
</rss>