<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K344  EB Fls problem in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K344-EB-Fls-problem/m-p/1915433#M38116</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/204444"&gt;@xuan&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The package you are using is ASR 21-11 (4.7) compliant. There have been some changes from ASR 4.4 to 4.7 (21-11). Here is a community post explaining the changes made:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/no-fee-and-fls-modules-in-RTD-of-s32k3x/td-p/1842835" target="_blank"&gt;Solved: no fee and fls modules in RTD of s32k3x - NXP Community&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;You can use the new modules (MemAcc, etc.) instead, or you can also download an ASR 4.4 version for the RTD package instead.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 23 Jul 2024 18:18:36 GMT</pubDate>
    <dc:creator>Julián_AragónM</dc:creator>
    <dc:date>2024-07-23T18:18:36Z</dc:date>
    <item>
      <title>S32K344  EB Fls problem</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-EB-Fls-problem/m-p/1914574#M38036</link>
      <description>&lt;P&gt;HI，&lt;/P&gt;&lt;P&gt;I installed a package of RTD4.0.0&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xuan_1-1721702672945.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/289814iB7FBF0174CE9DE50/image-size/medium?v=v2&amp;amp;px=400" alt="xuan_1-1721702672945.png" title="xuan_1-1721702672945.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;But I did not find the Fls module when I selected the module in EB&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xuan_2-1721702785208.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/289815iCC20666CF2A587F5/image-size/medium?v=v2&amp;amp;px=400" alt="xuan_2-1721702785208.png" title="xuan_2-1721702785208.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;There is also no folder for Fls under the RTD4.0.0 installation path&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xuan_3-1721702947391.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/289818i1B866F2E8D15282A/image-size/medium?v=v2&amp;amp;px=400" alt="xuan_3-1721702947391.png" title="xuan_3-1721702947391.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;What I want to know is that the RTD4.0.0 package itself does not support Fls module?&lt;/P&gt;&lt;P&gt;What do I need to do if I want to use the Fls module in this package of RTD4.0.0?&lt;/P&gt;&lt;P&gt;(The reason I use the package RTD4.0.0 is that it supports the FS26 module)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 23 Jul 2024 02:56:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-EB-Fls-problem/m-p/1914574#M38036</guid>
      <dc:creator>xuan</dc:creator>
      <dc:date>2024-07-23T02:56:54Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344  EB Fls problem</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-EB-Fls-problem/m-p/1915433#M38116</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/204444"&gt;@xuan&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The package you are using is ASR 21-11 (4.7) compliant. There have been some changes from ASR 4.4 to 4.7 (21-11). Here is a community post explaining the changes made:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/no-fee-and-fls-modules-in-RTD-of-s32k3x/td-p/1842835" target="_blank"&gt;Solved: no fee and fls modules in RTD of s32k3x - NXP Community&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;You can use the new modules (MemAcc, etc.) instead, or you can also download an ASR 4.4 version for the RTD package instead.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 23 Jul 2024 18:18:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-EB-Fls-problem/m-p/1915433#M38116</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-07-23T18:18:36Z</dc:date>
    </item>
  </channel>
</rss>