<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K144 IAR Project Build</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-IAR-Project-Build/m-p/1915191#M38078</link>
    <description>&lt;P&gt;I want to create an IAR project by following the S32DS routine about S32K144. After the project is compiled, I get an error when I enter debug mode. I also tried to export the xml file from the S32DS routine to create the project, again this error occurs, but it can be debug in S32DS.&lt;/P&gt;&lt;P&gt;This is the IAR project I created, which configuration items will have problems in the interim? Thanks for help&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Snipaste_2024-07-23_22-53-18.png" style="width: 543px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/289953iC31CDDF77EB2B348/image-size/large?v=v2&amp;amp;px=999" role="button" title="Snipaste_2024-07-23_22-53-18.png" alt="Snipaste_2024-07-23_22-53-18.png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 23 Jul 2024 14:58:26 GMT</pubDate>
    <dc:creator>Embedded_novice</dc:creator>
    <dc:date>2024-07-23T14:58:26Z</dc:date>
    <item>
      <title>S32K144 IAR Project Build</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-IAR-Project-Build/m-p/1915191#M38078</link>
      <description>&lt;P&gt;I want to create an IAR project by following the S32DS routine about S32K144. After the project is compiled, I get an error when I enter debug mode. I also tried to export the xml file from the S32DS routine to create the project, again this error occurs, but it can be debug in S32DS.&lt;/P&gt;&lt;P&gt;This is the IAR project I created, which configuration items will have problems in the interim? Thanks for help&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Snipaste_2024-07-23_22-53-18.png" style="width: 543px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/289953iC31CDDF77EB2B348/image-size/large?v=v2&amp;amp;px=999" role="button" title="Snipaste_2024-07-23_22-53-18.png" alt="Snipaste_2024-07-23_22-53-18.png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 23 Jul 2024 14:58:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-IAR-Project-Build/m-p/1915191#M38078</guid>
      <dc:creator>Embedded_novice</dc:creator>
      <dc:date>2024-07-23T14:58:26Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 IAR Project Build</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-IAR-Project-Build/m-p/1916421#M38193</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/213197"&gt;@Embedded_novice&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;This seems to be an issue with using J-Link instead of I&lt;SPAN&gt;-Jet. Please look at the following posts:&lt;/SPAN&gt;&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;&lt;SPAN&gt;&lt;A href="https://community.nxp.com/t5/S32K/S32K311-Stack-pointer-is-setup-to-incorrect-alignment/m-p/1862322" target="_blank"&gt;Solved: Re: S32K311 Stack pointer is setup to incorrect alignment - NXP Community&lt;/A&gt;&lt;/SPAN&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;SPAN&gt;&lt;A href="https://forum.segger.com/index.php/Thread/6610-SOLVED-Stack-pointer-is-setup-to-incorrect-alignment/" target="_blank"&gt;[SOLVED] Stack pointer is setup to incorrect alignment - J-Link/Flasher related - SEGGER - Forum&lt;/A&gt;&lt;/SPAN&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&lt;SPAN&gt;You could also try to export the project to IAR EW instead:&lt;/SPAN&gt;&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;&lt;SPAN&gt;&lt;A href="https://mp.weixin.qq.com/s?__biz=MzI0MDk0ODcxMw==&amp;amp;mid=2247486221&amp;amp;idx=1&amp;amp;sn=3ee2592c4610a3189ac323fe1f7c5a02&amp;amp;chksm=e9124f8bde65c69d0ac535864b773e540aee0212364a9d298021c0e89a97bc938db0e9406643&amp;amp;scene=21#wechat_redirect" target="_blank"&gt;S32K1xx Series MCU Application Development Guide - IAR toolchain Sample Engineering and Usage FAQ (qq.com)&lt;/A&gt;&lt;/SPAN&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;SPAN&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Export-S32DS-Project-to-IAR-EW-S32K14x-S32K11x/ta-p/1122428" target="_blank"&gt;HOWTO: Export S32DS Project to IAR EW (S32K14x/S32K11x) - NXP Community&lt;/A&gt;&lt;/SPAN&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;BR /&gt;Julián&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 24 Jul 2024 18:17:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-IAR-Project-Build/m-p/1916421#M38193</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-07-24T18:17:40Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 IAR Project Build</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-IAR-Project-Build/m-p/1916716#M38206</link>
      <description>Thanks for your help.</description>
      <pubDate>Thu, 25 Jul 2024 01:36:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-IAR-Project-Build/m-p/1916716#M38206</guid>
      <dc:creator>Embedded_novice</dc:creator>
      <dc:date>2024-07-25T01:36:33Z</dc:date>
    </item>
  </channel>
</rss>