<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックSpi data</title>
    <link>https://community.nxp.com/t5/S32K/Spi-data/m-p/1910613#M37791</link>
    <description>&lt;P&gt;Dear Tech Support&lt;/P&gt;&lt;P&gt;I am trying to communicate to UJA1169 and I am using 12 volt supply.&lt;/P&gt;&lt;P&gt;I am using Autosar standard for communication ,and&amp;nbsp; I have used Setup_Eb Apis for setting buffer and for transmission I have sent 0xFD,0xCF but in rx buffer I am getting 0xFF.&lt;/P&gt;&lt;P&gt;even I have changed value.&lt;/P&gt;&lt;P&gt;Can you explain the reason behind this?&lt;/P&gt;&lt;P&gt;B.R&lt;/P&gt;&lt;P&gt;Ashish&lt;/P&gt;</description>
    <pubDate>Wed, 17 Jul 2024 14:05:23 GMT</pubDate>
    <dc:creator>Ashish4525</dc:creator>
    <dc:date>2024-07-17T14:05:23Z</dc:date>
    <item>
      <title>Spi data</title>
      <link>https://community.nxp.com/t5/S32K/Spi-data/m-p/1910613#M37791</link>
      <description>&lt;P&gt;Dear Tech Support&lt;/P&gt;&lt;P&gt;I am trying to communicate to UJA1169 and I am using 12 volt supply.&lt;/P&gt;&lt;P&gt;I am using Autosar standard for communication ,and&amp;nbsp; I have used Setup_Eb Apis for setting buffer and for transmission I have sent 0xFD,0xCF but in rx buffer I am getting 0xFF.&lt;/P&gt;&lt;P&gt;even I have changed value.&lt;/P&gt;&lt;P&gt;Can you explain the reason behind this?&lt;/P&gt;&lt;P&gt;B.R&lt;/P&gt;&lt;P&gt;Ashish&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jul 2024 14:05:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Spi-data/m-p/1910613#M37791</guid>
      <dc:creator>Ashish4525</dc:creator>
      <dc:date>2024-07-17T14:05:23Z</dc:date>
    </item>
    <item>
      <title>Re: Spi data</title>
      <link>https://community.nxp.com/t5/S32K/Spi-data/m-p/1912263#M37852</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;could you please measure SPI signals with scope/analyzer to be sure what is sent? Also be sure right SPI protocol is used as mentioned in the UJA1169 datasheet.&lt;BR /&gt;An SPI read/write access must not be attempted for at least tto(SPI) after the UJA1169 exits &lt;BR /&gt;Reset mode (positive edge on RSTN).&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR, Petr&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 19 Jul 2024 12:17:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Spi-data/m-p/1912263#M37852</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-07-19T12:17:05Z</dc:date>
    </item>
    <item>
      <title>Re: Spi data</title>
      <link>https://community.nxp.com/t5/S32K/Spi-data/m-p/1913674#M37982</link>
      <description>&lt;P&gt;Dear PetrS&lt;/P&gt;&lt;P&gt;I am trying to run spi in synchronous mode. Do I have to enable SPI interrupt?&lt;/P&gt;&lt;P&gt;Note: I am running SPI on 40MHZ is it ok? In mOSi no data I am able to see now also TDR register no value is getting stored.&amp;nbsp;&lt;/P&gt;&lt;P&gt;B.R&lt;/P&gt;&lt;P&gt;Ashish&lt;/P&gt;</description>
      <pubDate>Mon, 22 Jul 2024 06:10:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Spi-data/m-p/1913674#M37982</guid>
      <dc:creator>Ashish4525</dc:creator>
      <dc:date>2024-07-22T06:10:24Z</dc:date>
    </item>
    <item>
      <title>Re: Spi data</title>
      <link>https://community.nxp.com/t5/S32K/Spi-data/m-p/1916081#M38161</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;for sync transmit SPI interrupt is not needed.&lt;BR /&gt;A 40MHz rate is quite high, depends on pins used. You can test lower rates first.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Wed, 24 Jul 2024 10:46:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Spi-data/m-p/1916081#M38161</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-07-24T10:46:19Z</dc:date>
    </item>
  </channel>
</rss>