<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: s32k314 Debug Hardware Questions</title>
    <link>https://community.nxp.com/t5/S32K/s32k314-Debug-Hardware-Questions/m-p/1910252#M37775</link>
    <description>&lt;P&gt;I looked at the S32K344 - Q172 board and drew it along the circuit.&lt;BR /&gt;This corresponds to PORTF among the photos you provided.&lt;BR /&gt;TDO, TDI, and RST have 5V output&lt;BR /&gt;The TCK is connected to the ground and outputs 0V.&lt;BR /&gt;However, TMS is connected to PTA4 with 1.5 to 1.6V output.&lt;/P&gt;</description>
    <pubDate>Wed, 17 Jul 2024 05:47:42 GMT</pubDate>
    <dc:creator>Oido</dc:creator>
    <dc:date>2024-07-17T05:47:42Z</dc:date>
    <item>
      <title>s32k314 Debug Hardware Questions</title>
      <link>https://community.nxp.com/t5/S32K/s32k314-Debug-Hardware-Questions/m-p/1874125#M35758</link>
      <description>&lt;P&gt;Hello, I am designing a PCB using S32K314. This is my first time designing a PCB and I am having a hard time. The debug equipment I am currently using is USB Multilink Universal, Rev. E. And I read Hardware Design Guides for S32K3XX Microcontrollers and drew an example circuit called JTAG connector with a CAD program.&lt;BR /&gt;But when I look at the manual of USB Multilink Universal, it says JTAG is 14PIN. What should I do?&lt;BR /&gt;Can I use other debug pins? And even if I can, there are no circuit guidelines in the Hardware Design Guides for S32K3XX Microcontrollers document to pack other debug pins. Please help. This is the JTAG I drew.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JTAG.jpg" style="width: 630px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/280581i6BDE2F6EAAC3D1F4/image-size/large?v=v2&amp;amp;px=999" role="button" title="JTAG.jpg" alt="JTAG.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 24 May 2024 01:33:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k314-Debug-Hardware-Questions/m-p/1874125#M35758</guid>
      <dc:creator>Oido</dc:creator>
      <dc:date>2024-05-24T01:33:01Z</dc:date>
    </item>
    <item>
      <title>Re: s32k314 Debug Hardware Questions</title>
      <link>https://community.nxp.com/t5/S32K/s32k314-Debug-Hardware-Questions/m-p/1874897#M35785</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/226367"&gt;@Oido&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The USB Multilink Universal and the&amp;nbsp;USB Multilink Universal FX have several debug headers&amp;nbsp;inside to support&amp;nbsp;NXP devices &amp;amp; other ARM Cortex microcontrollers. For S32K3 devices there are the PORT B (STANDARD ARM), PORT F (MINI 20), and&amp;nbsp;PORT G (MINI 10).&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="VaneB_2-1716584629198.png" style="width: 226px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/280815i80B349123D9FA022/image-dimensions/226x247?v=v2" width="226" height="247" role="button" title="VaneB_2-1716584629198.png" alt="VaneB_2-1716584629198.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="VaneB_1-1716584500902.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/280813i165377B72E6DB0BD/image-dimensions/400x300?v=v2" width="400" height="300" role="button" title="VaneB_1-1716584500902.png" alt="VaneB_1-1716584500902.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;So, we recommend following the&amp;nbsp;circuit guidelines provided in section&amp;nbsp;4.2 (JTAG and TRACE interface) of the Hardware Design Guides for S32K3XX Microcontrollers. You can also use as a reference the S32K3&amp;nbsp;Evaluation Board's schematics.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R.&lt;/P&gt;
&lt;P&gt;VaneB&lt;/P&gt;</description>
      <pubDate>Fri, 24 May 2024 21:10:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k314-Debug-Hardware-Questions/m-p/1874897#M35785</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2024-05-24T21:10:03Z</dc:date>
    </item>
    <item>
      <title>Re: s32k314 Debug Hardware Questions</title>
      <link>https://community.nxp.com/t5/S32K/s32k314-Debug-Hardware-Questions/m-p/1910252#M37775</link>
      <description>&lt;P&gt;I looked at the S32K344 - Q172 board and drew it along the circuit.&lt;BR /&gt;This corresponds to PORTF among the photos you provided.&lt;BR /&gt;TDO, TDI, and RST have 5V output&lt;BR /&gt;The TCK is connected to the ground and outputs 0V.&lt;BR /&gt;However, TMS is connected to PTA4 with 1.5 to 1.6V output.&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jul 2024 05:47:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k314-Debug-Hardware-Questions/m-p/1910252#M37775</guid>
      <dc:creator>Oido</dc:creator>
      <dc:date>2024-07-17T05:47:42Z</dc:date>
    </item>
  </channel>
</rss>