<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: s32k3 hse api compatibility problem</title>
    <link>https://community.nxp.com/t5/S32K/s32k3-hse-api-compatibility-problem/m-p/1909332#M37745</link>
    <description>&lt;P&gt;Hi&amp;nbsp;victory,&lt;/P&gt;
&lt;P&gt;Which HSE examples did you download? If you mean &lt;STRONG&gt;SecureBootAppNoteDemo&lt;/STRONG&gt; &lt;EM&gt;SW745310&lt;/EM&gt;, then please take a look at&amp;nbsp;&lt;STRONG&gt;Hse_Ip_ServiceRequest.&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;RTD has just a few HSE functions in Ip layer. You can take a look at:&lt;BR /&gt;C:\NXP\S32DS.3.5_RTD400\S32DS\software\PlatformSDK_S32K3\RTD\Crypto_TS_T40D34M40I0R0\doc\RTD_CRYPTO_UM.pdf&lt;/P&gt;
&lt;P&gt;These functions are used by the framework. For example, framework function &lt;STRONG&gt;HSE_Send&lt;/STRONG&gt;() uses function &lt;STRONG&gt;Hse_Ip_ServiceRequest&lt;/STRONG&gt;() from HSE Ip layer (see hse_host.c file).&lt;/P&gt;
&lt;P&gt;So, you need to add the framework files, HSE FW interface files as described in the integration manual and then you can re-use code from the demo. (C:\NXP\S32DS.3.5_RTD400\S32DS\software\PlatformSDK_S32K3\RTD\Crypto_TS_T40D34M40I0R0\doc\RTD_CRYPTO_IM.pdf)&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Tue, 16 Jul 2024 03:29:56 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2024-07-16T03:29:56Z</dc:date>
    <item>
      <title>s32k3 hse api compatibility problem</title>
      <link>https://community.nxp.com/t5/S32K/s32k3-hse-api-compatibility-problem/m-p/1906722#M37617</link>
      <description>&lt;P&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;i've used S32K312,&amp;nbsp; firmware 02.40,&amp;nbsp; S32K3_RTD_4_0_0_D2311_ASR_REL_4_7_REV_0000_20231128&amp;nbsp; sdk.&amp;nbsp; i download serveral hse example and see they all based on HSE_Send() call ,but it's not in my SDK, i could only found a symmetric example based on MCAL in IDE.&lt;/P&gt;&lt;P&gt;&amp;nbsp;so, what the difference between them? how could i import these&amp;nbsp; HSE_Send based example to my project? is there and additional work to do,like some init or address convertion ?&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 12 Jul 2024 03:41:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k3-hse-api-compatibility-problem/m-p/1906722#M37617</guid>
      <dc:creator>victory</dc:creator>
      <dc:date>2024-07-12T03:41:38Z</dc:date>
    </item>
    <item>
      <title>Re: s32k3 hse api compatibility problem</title>
      <link>https://community.nxp.com/t5/S32K/s32k3-hse-api-compatibility-problem/m-p/1909332#M37745</link>
      <description>&lt;P&gt;Hi&amp;nbsp;victory,&lt;/P&gt;
&lt;P&gt;Which HSE examples did you download? If you mean &lt;STRONG&gt;SecureBootAppNoteDemo&lt;/STRONG&gt; &lt;EM&gt;SW745310&lt;/EM&gt;, then please take a look at&amp;nbsp;&lt;STRONG&gt;Hse_Ip_ServiceRequest.&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;RTD has just a few HSE functions in Ip layer. You can take a look at:&lt;BR /&gt;C:\NXP\S32DS.3.5_RTD400\S32DS\software\PlatformSDK_S32K3\RTD\Crypto_TS_T40D34M40I0R0\doc\RTD_CRYPTO_UM.pdf&lt;/P&gt;
&lt;P&gt;These functions are used by the framework. For example, framework function &lt;STRONG&gt;HSE_Send&lt;/STRONG&gt;() uses function &lt;STRONG&gt;Hse_Ip_ServiceRequest&lt;/STRONG&gt;() from HSE Ip layer (see hse_host.c file).&lt;/P&gt;
&lt;P&gt;So, you need to add the framework files, HSE FW interface files as described in the integration manual and then you can re-use code from the demo. (C:\NXP\S32DS.3.5_RTD400\S32DS\software\PlatformSDK_S32K3\RTD\Crypto_TS_T40D34M40I0R0\doc\RTD_CRYPTO_IM.pdf)&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 16 Jul 2024 03:29:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k3-hse-api-compatibility-problem/m-p/1909332#M37745</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-07-16T03:29:56Z</dc:date>
    </item>
  </channel>
</rss>