<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: LPSPI_DRV_MasterStartTransfer()</title>
    <link>https://community.nxp.com/t5/S32K/LPSPI-DRV-MasterStartTransfer/m-p/1905899#M37521</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;This function can be found in&amp;nbsp;.../SDK/platform/drivers/src/lpspi/lpspi_master_driver.c and it is &lt;STRONG&gt;static&lt;/STRONG&gt; status_t LPSPI_DRV_MasterStartTransfer()&lt;/P&gt;
&lt;P&gt;Why not use&amp;nbsp;LPSPI_DRV_MasterTransfer or&amp;nbsp;LPSPI_DRV_MasterTransferBlocking?&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Thu, 11 Jul 2024 06:29:26 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2024-07-11T06:29:26Z</dc:date>
    <item>
      <title>LPSPI_DRV_MasterStartTransfer()</title>
      <link>https://community.nxp.com/t5/S32K/LPSPI-DRV-MasterStartTransfer/m-p/1905547#M37501</link>
      <description>&lt;P&gt;Disclaimer: I am fairly new to S32DS&lt;/P&gt;&lt;P&gt;I was given a repository of code from a project that hasn't been touched in a long time. Upon opening the project, I was greeted with this error. When hovering my mouse over the error, it says "undefined reference to&amp;nbsp;LPSPI_DRV_MasterStartTransfer". I am using ARM v2.0 as that is what the code was written in. Do I need to download any extra libraries, SDKs or drivers to make this code work?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Code Error 1.PNG" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/287990i1F8A23BFACC9640D/image-size/large?v=v2&amp;amp;px=999" role="button" title="Code Error 1.PNG" alt="Code Error 1.PNG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Code Error 1.PNG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 10 Jul 2024 19:31:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPSPI-DRV-MasterStartTransfer/m-p/1905547#M37501</guid>
      <dc:creator>DevinHolz</dc:creator>
      <dc:date>2024-07-10T19:31:56Z</dc:date>
    </item>
    <item>
      <title>Re: LPSPI_DRV_MasterStartTransfer()</title>
      <link>https://community.nxp.com/t5/S32K/LPSPI-DRV-MasterStartTransfer/m-p/1905899#M37521</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;This function can be found in&amp;nbsp;.../SDK/platform/drivers/src/lpspi/lpspi_master_driver.c and it is &lt;STRONG&gt;static&lt;/STRONG&gt; status_t LPSPI_DRV_MasterStartTransfer()&lt;/P&gt;
&lt;P&gt;Why not use&amp;nbsp;LPSPI_DRV_MasterTransfer or&amp;nbsp;LPSPI_DRV_MasterTransferBlocking?&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 11 Jul 2024 06:29:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPSPI-DRV-MasterStartTransfer/m-p/1905899#M37521</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-07-11T06:29:26Z</dc:date>
    </item>
    <item>
      <title>Re: LPSPI_DRV_MasterStartTransfer()</title>
      <link>https://community.nxp.com/t5/S32K/LPSPI-DRV-MasterStartTransfer/m-p/1906369#M37583</link>
      <description>Thank you. I added an include to that C file which seemed to do the trick.&lt;BR /&gt;&lt;BR /&gt;As for why that command is used, I don't know. I was simply given this repository with very little notation so I'm not sure how anything works.</description>
      <pubDate>Thu, 11 Jul 2024 13:59:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPSPI-DRV-MasterStartTransfer/m-p/1906369#M37583</guid>
      <dc:creator>DevinHolz</dc:creator>
      <dc:date>2024-07-11T13:59:47Z</dc:date>
    </item>
  </channel>
</rss>