<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K344 Flash operation and interrupt in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K344-Flash-operation-and-interrupt/m-p/1905879#M37519</link>
    <description>&lt;P&gt;Hello,I have question about When DFlash/PFlash is doing the write or erase operation,all interrupts must be disabled for awhile?&lt;/P&gt;&lt;P&gt;For example,disable all interrupts before&amp;nbsp;C40_Ip_MainInterfaceSectorErase() or&amp;nbsp;C40_Ip_MainInterfaceWrite(),then enable all interrupts&amp;nbsp;when operation is done.&lt;/P&gt;&lt;P&gt;Is there have any problem if the all interrupt is not disabled?&lt;/P&gt;</description>
    <pubDate>Thu, 11 Jul 2024 05:55:03 GMT</pubDate>
    <dc:creator>KWay4329</dc:creator>
    <dc:date>2024-07-11T05:55:03Z</dc:date>
    <item>
      <title>S32K344 Flash operation and interrupt</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-Flash-operation-and-interrupt/m-p/1905879#M37519</link>
      <description>&lt;P&gt;Hello,I have question about When DFlash/PFlash is doing the write or erase operation,all interrupts must be disabled for awhile?&lt;/P&gt;&lt;P&gt;For example,disable all interrupts before&amp;nbsp;C40_Ip_MainInterfaceSectorErase() or&amp;nbsp;C40_Ip_MainInterfaceWrite(),then enable all interrupts&amp;nbsp;when operation is done.&lt;/P&gt;&lt;P&gt;Is there have any problem if the all interrupt is not disabled?&lt;/P&gt;</description>
      <pubDate>Thu, 11 Jul 2024 05:55:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-Flash-operation-and-interrupt/m-p/1905879#M37519</guid>
      <dc:creator>KWay4329</dc:creator>
      <dc:date>2024-07-11T05:55:03Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 Flash operation and interrupt</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-Flash-operation-and-interrupt/m-p/1908844#M37727</link>
      <description>&lt;P&gt;If code is being executed from different flash module than programmed (RWW) then interrupts can be handled during flash programming otherwise it is needed to disable interrupt before flash programming/erasing to prevent RWW error.&lt;/P&gt;</description>
      <pubDate>Mon, 15 Jul 2024 13:23:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-Flash-operation-and-interrupt/m-p/1908844#M37727</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2024-07-15T13:23:01Z</dc:date>
    </item>
  </channel>
</rss>