<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K311 SPI DMA in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K311-SPI-DMA/m-p/1905755#M37512</link>
    <description>&lt;P&gt;&lt;SPAN&gt;S32K311 is configured with SPI DMA, but if the DMA channels use 4 and 5, then SPI can trigger a DMA interrupt. If you use other channels, then it will not work. For example, channels 0, 1, 2 and 3 will not work. Use EB to configure it here, RTD3.0. I want to ask why. Thank you. If you want to project, I can upload it.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 11 Jul 2024 02:09:59 GMT</pubDate>
    <dc:creator>Jon123</dc:creator>
    <dc:date>2024-07-11T02:09:59Z</dc:date>
    <item>
      <title>S32K311 SPI DMA</title>
      <link>https://community.nxp.com/t5/S32K/S32K311-SPI-DMA/m-p/1905755#M37512</link>
      <description>&lt;P&gt;&lt;SPAN&gt;S32K311 is configured with SPI DMA, but if the DMA channels use 4 and 5, then SPI can trigger a DMA interrupt. If you use other channels, then it will not work. For example, channels 0, 1, 2 and 3 will not work. Use EB to configure it here, RTD3.0. I want to ask why. Thank you. If you want to project, I can upload it.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 11 Jul 2024 02:09:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K311-SPI-DMA/m-p/1905755#M37512</guid>
      <dc:creator>Jon123</dc:creator>
      <dc:date>2024-07-11T02:09:59Z</dc:date>
    </item>
    <item>
      <title>Re: S32K311 SPI DMA</title>
      <link>https://community.nxp.com/t5/S32K/S32K311-SPI-DMA/m-p/1905757#M37513</link>
      <description>&lt;DIV class=""&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;To add, what's interesting is that this will not happen to the S32K312&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Thu, 11 Jul 2024 02:12:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K311-SPI-DMA/m-p/1905757#M37513</guid>
      <dc:creator>Jon123</dc:creator>
      <dc:date>2024-07-11T02:12:05Z</dc:date>
    </item>
    <item>
      <title>Re: S32K311 SPI DMA</title>
      <link>https://community.nxp.com/t5/S32K/S32K311-SPI-DMA/m-p/1907035#M37632</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/227778"&gt;@Jon123&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Can you please share the whole project, the configuration and the code?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you,&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
      <pubDate>Fri, 12 Jul 2024 10:41:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K311-SPI-DMA/m-p/1907035#M37632</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2024-07-12T10:41:42Z</dc:date>
    </item>
  </channel>
</rss>