<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K144 Development kit no longer uploads. in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-Development-kit-no-longer-uploads/m-p/862020#M3751</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mike,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm working with Matt on this. I have checked J107 and the jumper is in the correct position. We did switch its position at one point to update the P&amp;amp;E firmware but it is back to being in the 2-3 position.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This issue first arose while uploading programs using the NXP Model-Based Design Toolbox in Simulink.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 01 Apr 2019 19:20:29 GMT</pubDate>
    <dc:creator>pdom</dc:creator>
    <dc:date>2019-04-01T19:20:29Z</dc:date>
    <item>
      <title>S32K144 Development kit no longer uploads.</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-Development-kit-no-longer-uploads/m-p/862018#M3749</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/mikedoidge"&gt;mikedoidge&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have 3 S32k144 development boards that are in a bricked state, this occurred unexpectedly and the boards had no problems before. We have no problem uploading to most of our boards but these three have issues, the reset LED is not high. We are able to recognize the broken boards on the windows explorer but unable to upload to them. Here is the error we receive in S32K design studio.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/79154iBE69C1108136FB5F/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When hitting retry, we see the reset LED flash but the error pops back up. The rest of our development boards upload without issue. We have tried updating the&amp;nbsp;P&amp;amp;E micro firmware in the boot loader but this has not helped.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We also tried to upload a previously built .mot file to the board over windows explorer but that had no effect (although the files transferred without issue)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This problem&amp;nbsp;appeared while uploading auto-generated code from the NXP simulation library for the S32K.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Mar 2019 23:22:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-Development-kit-no-longer-uploads/m-p/862018#M3749</guid>
      <dc:creator>mattdr</dc:creator>
      <dc:date>2019-03-28T23:22:13Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 Development kit no longer uploads.</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-Development-kit-no-longer-uploads/m-p/862019#M3750</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/matthewdreisbach"&gt;matthewdreisbach&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did you change J107 on the affected boards? This should be 2-3 not 1-2. Having this jumper set wrong could cause this exact issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Mar 2019 20:56:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-Development-kit-no-longer-uploads/m-p/862019#M3750</guid>
      <dc:creator>mikedoidge</dc:creator>
      <dc:date>2019-03-29T20:56:54Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 Development kit no longer uploads.</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-Development-kit-no-longer-uploads/m-p/862020#M3751</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mike,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm working with Matt on this. I have checked J107 and the jumper is in the correct position. We did switch its position at one point to update the P&amp;amp;E firmware but it is back to being in the 2-3 position.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This issue first arose while uploading programs using the NXP Model-Based Design Toolbox in Simulink.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Apr 2019 19:20:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-Development-kit-no-longer-uploads/m-p/862020#M3751</guid>
      <dc:creator>pdom</dc:creator>
      <dc:date>2019-04-01T19:20:29Z</dc:date>
    </item>
  </channel>
</rss>