<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックFlexCAN Polling</title>
    <link>https://community.nxp.com/t5/S32K/FlexCAN-Polling/m-p/1902313#M37305</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;Is there an example of using the FlexCAN APIs for polling?&lt;BR /&gt;&lt;BR /&gt;How do I use the following APIs:&lt;/P&gt;&lt;P&gt;-&amp;nbsp;FlexCAN_Ip_MainFunctionWrite&lt;/P&gt;&lt;P&gt;-&amp;nbsp;FlexCAN_Ip_MainFunctionRead&lt;/P&gt;&lt;P&gt;-&amp;nbsp;FlexCAN_Ip_Send&lt;/P&gt;&lt;P&gt;-&amp;nbsp;FlexCAN_Ip_Receive&lt;BR /&gt;&lt;BR /&gt;Could you provide an example using the APIs, with the configuration set for CAN FD by using the polling method?&lt;/P&gt;</description>
    <pubDate>Mon, 08 Jul 2024 13:22:04 GMT</pubDate>
    <dc:creator>Samuel_DCosta</dc:creator>
    <dc:date>2024-07-08T13:22:04Z</dc:date>
    <item>
      <title>FlexCAN Polling</title>
      <link>https://community.nxp.com/t5/S32K/FlexCAN-Polling/m-p/1902313#M37305</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;Is there an example of using the FlexCAN APIs for polling?&lt;BR /&gt;&lt;BR /&gt;How do I use the following APIs:&lt;/P&gt;&lt;P&gt;-&amp;nbsp;FlexCAN_Ip_MainFunctionWrite&lt;/P&gt;&lt;P&gt;-&amp;nbsp;FlexCAN_Ip_MainFunctionRead&lt;/P&gt;&lt;P&gt;-&amp;nbsp;FlexCAN_Ip_Send&lt;/P&gt;&lt;P&gt;-&amp;nbsp;FlexCAN_Ip_Receive&lt;BR /&gt;&lt;BR /&gt;Could you provide an example using the APIs, with the configuration set for CAN FD by using the polling method?&lt;/P&gt;</description>
      <pubDate>Mon, 08 Jul 2024 13:22:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FlexCAN-Polling/m-p/1902313#M37305</guid>
      <dc:creator>Samuel_DCosta</dc:creator>
      <dc:date>2024-07-08T13:22:04Z</dc:date>
    </item>
    <item>
      <title>Re: FlexCAN Polling</title>
      <link>https://community.nxp.com/t5/S32K/FlexCAN-Polling/m-p/1902921#M37333</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/221691"&gt;@Samuel_DCosta&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;You can find a reference example for normal/user mode in polling mode for the S32K312 derivative:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-CAN-Transmit-amp-Receive-Using-Polling-mode-DS3/ta-p/1789191" target="_blank"&gt;Example S32K312 CAN Transmit &amp;amp; Receive Using Polling mode DS3.5 RTD300 - NXP Community&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;The FlexCAN_Ip_Example from the RTD package uses the APIs as well (&lt;STRONG&gt;FlexCAN_Ip_Init&lt;/STRONG&gt; will configure for loopback the FlexCAN0 and then application will send through ISR and receive as polling.).&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
      <pubDate>Mon, 08 Jul 2024 20:03:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FlexCAN-Polling/m-p/1902921#M37333</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-07-08T20:03:59Z</dc:date>
    </item>
  </channel>
</rss>