<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can Rx issue in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Can-Rx-issue/m-p/1898353#M37145</link>
    <description>&lt;P&gt;Dear Peter&lt;/P&gt;&lt;P&gt;When I am trying to send data in 20TQ it is not going but at 23Tq and 24Tq it is going .&lt;/P&gt;&lt;P&gt;baud rate 500Kpbs and 40MHZ clock with 4 prescale , So time quanta will come 20 but no frame is being transmitting.&lt;/P&gt;&lt;P&gt;B.R&lt;/P&gt;&lt;P&gt;Ashish&lt;/P&gt;</description>
    <pubDate>Wed, 03 Jul 2024 11:05:25 GMT</pubDate>
    <dc:creator>Ashish4525</dc:creator>
    <dc:date>2024-07-03T11:05:25Z</dc:date>
    <item>
      <title>Can Rx issue</title>
      <link>https://community.nxp.com/t5/S32K/Can-Rx-issue/m-p/1896630#M37048</link>
      <description>&lt;P&gt;Dear all&lt;/P&gt;&lt;P&gt;I am trying run CAN on S32k118evb2Q048,I can able to transmitt using Can_Write. but when I am unable to receive via CAN analyzer .it shows erros which I have shared with you in attachment.&lt;/P&gt;&lt;P&gt;Also I have added canISR in startup code ,still it is not hittng.&lt;/P&gt;&lt;P&gt;All errors like CRC,ACK,stuff error only in receving time.&lt;/P&gt;&lt;P&gt;Both RX and TX are configured in interrupt.&lt;/P&gt;&lt;P&gt;Also Canif_RxIndication is not hitting too.&lt;/P&gt;&lt;P&gt;I have configured Rxfifo too in tresos with identfier 942 and mask is 2047.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 01 Jul 2024 11:17:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-Rx-issue/m-p/1896630#M37048</guid>
      <dc:creator>Ashish4525</dc:creator>
      <dc:date>2024-07-01T11:17:22Z</dc:date>
    </item>
    <item>
      <title>Re: Can Rx issue</title>
      <link>https://community.nxp.com/t5/S32K/Can-Rx-issue/m-p/1897218#M37084</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;simply message is not properly sent without error detected.&lt;BR /&gt;Generally, be sure CAN transceiver is active and properly terminated. Check if CAN bit rate is properly set and it is same for all nodes connected. Use SOSC clk for PE clock.&lt;BR /&gt;You can try to measure TX/RX and CAN bus signal to be sure it is expected one.&lt;/P&gt;
&lt;P&gt;BR, Petr&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jul 2024 06:53:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-Rx-issue/m-p/1897218#M37084</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-07-02T06:53:41Z</dc:date>
    </item>
    <item>
      <title>Re: Can Rx issue</title>
      <link>https://community.nxp.com/t5/S32K/Can-Rx-issue/m-p/1897286#M37087</link>
      <description>&lt;P&gt;Dear Petr&lt;/P&gt;&lt;P&gt;SOSC I am using for CAN and bit rate is also set with 20TQ and 500 kbps baud rate with 40MHZ clock and 4 prescaller.&lt;/P&gt;&lt;P&gt;B.R&lt;/P&gt;&lt;P&gt;Ashish&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jul 2024 07:55:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-Rx-issue/m-p/1897286#M37087</guid>
      <dc:creator>Ashish4525</dc:creator>
      <dc:date>2024-07-02T07:55:54Z</dc:date>
    </item>
    <item>
      <title>Re: Can Rx issue</title>
      <link>https://community.nxp.com/t5/S32K/Can-Rx-issue/m-p/1897339#M37090</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;yes, this option is possible, but errors are detected, so check real signals, sample point used and bus terminations.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jul 2024 09:01:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-Rx-issue/m-p/1897339#M37090</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-07-02T09:01:54Z</dc:date>
    </item>
    <item>
      <title>Re: Can Rx issue</title>
      <link>https://community.nxp.com/t5/S32K/Can-Rx-issue/m-p/1898353#M37145</link>
      <description>&lt;P&gt;Dear Peter&lt;/P&gt;&lt;P&gt;When I am trying to send data in 20TQ it is not going but at 23Tq and 24Tq it is going .&lt;/P&gt;&lt;P&gt;baud rate 500Kpbs and 40MHZ clock with 4 prescale , So time quanta will come 20 but no frame is being transmitting.&lt;/P&gt;&lt;P&gt;B.R&lt;/P&gt;&lt;P&gt;Ashish&lt;/P&gt;</description>
      <pubDate>Wed, 03 Jul 2024 11:05:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-Rx-issue/m-p/1898353#M37145</guid>
      <dc:creator>Ashish4525</dc:creator>
      <dc:date>2024-07-03T11:05:25Z</dc:date>
    </item>
    <item>
      <title>Re: Can Rx issue</title>
      <link>https://community.nxp.com/t5/S32K/Can-Rx-issue/m-p/1898358#M37147</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;seems your PE clock is running from FIRC (system clock) and not from crystal. Check CTRL1[SRCCLK] setting and config bit timing accordingly.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Wed, 03 Jul 2024 11:15:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-Rx-issue/m-p/1898358#M37147</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-07-03T11:15:35Z</dc:date>
    </item>
    <item>
      <title>Re: Can Rx issue</title>
      <link>https://community.nxp.com/t5/S32K/Can-Rx-issue/m-p/1898369#M37148</link>
      <description>&lt;P&gt;HI&lt;/P&gt;&lt;P&gt;Please See PFA I am using SOSC with 40mhz&lt;/P&gt;&lt;P&gt;B.R&lt;/P&gt;&lt;P&gt;Ashish&lt;/P&gt;</description>
      <pubDate>Wed, 03 Jul 2024 11:35:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-Rx-issue/m-p/1898369#M37148</guid>
      <dc:creator>Ashish4525</dc:creator>
      <dc:date>2024-07-03T11:35:36Z</dc:date>
    </item>
    <item>
      <title>Re: Can Rx issue</title>
      <link>https://community.nxp.com/t5/S32K/Can-Rx-issue/m-p/1898378#M37150</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;clock1.png shows CTRL1[CLKSRC] checked, so if this is really set, then PE clock is derived from SYSCLK. Is then SYSCLK running from SOSC or FIRC?&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 03 Jul 2024 11:46:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-Rx-issue/m-p/1898378#M37150</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-07-03T11:46:46Z</dc:date>
    </item>
    <item>
      <title>Re: Can Rx issue</title>
      <link>https://community.nxp.com/t5/S32K/Can-Rx-issue/m-p/1898389#M37151</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;It is running from SOSC&lt;/P&gt;&lt;P&gt;B.R&lt;/P&gt;&lt;P&gt;Ashish&lt;/P&gt;</description>
      <pubDate>Wed, 03 Jul 2024 12:10:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-Rx-issue/m-p/1898389#M37151</guid>
      <dc:creator>Ashish4525</dc:creator>
      <dc:date>2024-07-03T12:10:29Z</dc:date>
    </item>
  </channel>
</rss>