<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックWhen ConfigureAdvancedSecureBoot, the HSE_MU_GetHseStatus value is always the same.</title>
    <link>https://community.nxp.com/t5/S32K/When-ConfigureAdvancedSecureBoot-the-HSE-MU-GetHseStatus-value/m-p/1898028#M37127</link>
    <description>&lt;P&gt;Dear All.&lt;/P&gt;&lt;P&gt;Debugging with ConfigureAdvancedSecureBoot.&lt;BR /&gt;If InstallSMR or HSE_InstallCoreResetEntry is successful, the secure boot related bit is not toggled when HSE status is retrieved.&lt;BR /&gt;(However, it is normal when ConfigureSHESecurureBoot is used.)&lt;BR /&gt;Is this behavior intended? Why not support ConfigureAdvancedSecureBoot?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 03 Jul 2024 05:59:04 GMT</pubDate>
    <dc:creator>squirrel_rin</dc:creator>
    <dc:date>2024-07-03T05:59:04Z</dc:date>
    <item>
      <title>When ConfigureAdvancedSecureBoot, the HSE_MU_GetHseStatus value is always the same.</title>
      <link>https://community.nxp.com/t5/S32K/When-ConfigureAdvancedSecureBoot-the-HSE-MU-GetHseStatus-value/m-p/1898028#M37127</link>
      <description>&lt;P&gt;Dear All.&lt;/P&gt;&lt;P&gt;Debugging with ConfigureAdvancedSecureBoot.&lt;BR /&gt;If InstallSMR or HSE_InstallCoreResetEntry is successful, the secure boot related bit is not toggled when HSE status is retrieved.&lt;BR /&gt;(However, it is normal when ConfigureSHESecurureBoot is used.)&lt;BR /&gt;Is this behavior intended? Why not support ConfigureAdvancedSecureBoot?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 03 Jul 2024 05:59:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/When-ConfigureAdvancedSecureBoot-the-HSE-MU-GetHseStatus-value/m-p/1898028#M37127</guid>
      <dc:creator>squirrel_rin</dc:creator>
      <dc:date>2024-07-03T05:59:04Z</dc:date>
    </item>
    <item>
      <title>Re: When ConfigureAdvancedSecureBoot, the HSE_MU_GetHseStatus value is always the same.</title>
      <link>https://community.nxp.com/t5/S32K/When-ConfigureAdvancedSecureBoot-the-HSE-MU-GetHseStatus-value/m-p/1904265#M37436</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/234878"&gt;@squirrel_rin&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;different status bits are used for SHE secure boot and Advanced secure boot. Isn't that the problem? From Secure boot app note:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="lukaszadrapa_0-1720524792440.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/287779iC2539D535AB7707C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="lukaszadrapa_0-1720524792440.png" alt="lukaszadrapa_0-1720524792440.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;lukaszadrapa_0-1720524792440.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Tue, 09 Jul 2024 11:36:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/When-ConfigureAdvancedSecureBoot-the-HSE-MU-GetHseStatus-value/m-p/1904265#M37436</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2024-07-09T11:36:23Z</dc:date>
    </item>
  </channel>
</rss>