<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: S32K118</title>
    <link>https://community.nxp.com/t5/S32K/S32K118/m-p/859499#M3707</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm not sure about your described settings.&amp;nbsp;Could you please share your code?&lt;BR /&gt;In the RM, we can see "When software trigger is selected, a conversion is initiated following a write to SC1A."&lt;/P&gt;&lt;P&gt;So, the&amp;nbsp;&lt;SPAN&gt;software trigger can be used&amp;nbsp;&lt;/SPAN&gt;only for the SC1A.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the case, when you want to trigger more channels I would like to recommend to you the example S32K144 PDB ADC trigger DMA ISR S32DS&amp;nbsp;&lt;A href="https://community.nxp.com/docs/DOC-333054"&gt;Example S32K144 PDB ADC trigger DMA ISR S32DS&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, you can look at the examples in the S32DS.R1&amp;nbsp; &lt;EM&gt;File -&amp;gt; New -&amp;gt; S32DS Project from the Example.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 29 Jan 2019 10:18:39 GMT</pubDate>
    <dc:creator>dianabatrlova</dc:creator>
    <dc:date>2019-01-29T10:18:39Z</dc:date>
    <item>
      <title>S32K118</title>
      <link>https://community.nxp.com/t5/S32K/S32K118/m-p/859498#M3706</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to Know&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;FTM module which generates interrupt after every 100ms&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;I have included the ADC software trigger code in the same example code, where software triggers the ADC0 (CH12) to start it's conversion in the FTM interrupt&amp;nbsp;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This code is working with ADC0 CH12 as well as CH9 but when I tried to do the same on CH3 it didn't work.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As per reference manual ADC0 CH0-3 requires different triggering method, since we do not have any example code for it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you tell us-&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;What steps we should follow to configure those ADC0 CH0-3&lt;/LI&gt;&lt;LI&gt;Is that ok, if we used different triggering scheme for CH0-3 and different one for other channels of same ADC&lt;/LI&gt;&lt;/OL&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jan 2019 12:19:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K118/m-p/859498#M3706</guid>
      <dc:creator>akankshasrivast</dc:creator>
      <dc:date>2019-01-24T12:19:48Z</dc:date>
    </item>
    <item>
      <title>Re: S32K118</title>
      <link>https://community.nxp.com/t5/S32K/S32K118/m-p/859499#M3707</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm not sure about your described settings.&amp;nbsp;Could you please share your code?&lt;BR /&gt;In the RM, we can see "When software trigger is selected, a conversion is initiated following a write to SC1A."&lt;/P&gt;&lt;P&gt;So, the&amp;nbsp;&lt;SPAN&gt;software trigger can be used&amp;nbsp;&lt;/SPAN&gt;only for the SC1A.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the case, when you want to trigger more channels I would like to recommend to you the example S32K144 PDB ADC trigger DMA ISR S32DS&amp;nbsp;&lt;A href="https://community.nxp.com/docs/DOC-333054"&gt;Example S32K144 PDB ADC trigger DMA ISR S32DS&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, you can look at the examples in the S32DS.R1&amp;nbsp; &lt;EM&gt;File -&amp;gt; New -&amp;gt; S32DS Project from the Example.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Jan 2019 10:18:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K118/m-p/859499#M3707</guid>
      <dc:creator>dianabatrlova</dc:creator>
      <dc:date>2019-01-29T10:18:39Z</dc:date>
    </item>
  </channel>
</rss>