<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックWhy LCU is used for PWM?</title>
    <link>https://community.nxp.com/t5/S32K/Why-LCU-is-used-for-PWM/m-p/1896708#M37055</link>
    <description>&lt;P&gt;Do and why we need to route eMios PWM to LCU through TRGMUX?&lt;/P&gt;&lt;P&gt;What advantages does LCU provides?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using RTD (3.0.0) with non-autosar.&lt;/P&gt;</description>
    <pubDate>Mon, 01 Jul 2024 13:40:13 GMT</pubDate>
    <dc:creator>anakha</dc:creator>
    <dc:date>2024-07-01T13:40:13Z</dc:date>
    <item>
      <title>Why LCU is used for PWM?</title>
      <link>https://community.nxp.com/t5/S32K/Why-LCU-is-used-for-PWM/m-p/1896708#M37055</link>
      <description>&lt;P&gt;Do and why we need to route eMios PWM to LCU through TRGMUX?&lt;/P&gt;&lt;P&gt;What advantages does LCU provides?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using RTD (3.0.0) with non-autosar.&lt;/P&gt;</description>
      <pubDate>Mon, 01 Jul 2024 13:40:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Why-LCU-is-used-for-PWM/m-p/1896708#M37055</guid>
      <dc:creator>anakha</dc:creator>
      <dc:date>2024-07-01T13:40:13Z</dc:date>
    </item>
    <item>
      <title>Re: Why LCU is used for PWM?</title>
      <link>https://community.nxp.com/t5/S32K/Why-LCU-is-used-for-PWM/m-p/1897771#M37110</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/222923"&gt;@anakha&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;Do and why we need to route eMios PWM to LCU through TRGMUX?&lt;/STRONG&gt; The Enhanced Modular IO Subsystem (eMIOS), Logic Control Unit (LCU), Trigger MUX (TRGMUX), Body Cross-triggering Unit (BCTU) and Analogue-to-Digital Converter (ADC)&amp;nbsp;are directly interconnected and can be configured to meet various application requirements.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;More information related to the modules interconnection you can refer to&amp;nbsp;Motor Control application notes.&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/Download?colCode=AN13902" target="_blank" rel="noopener"&gt;AN13902&lt;/A&gt;,&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/Download?colCode=AN13884" target="_blank" rel="noopener"&gt;AN13884&lt;/A&gt; or&amp;nbsp;&lt;SPAN&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=AN13767" target="_blank" rel="noopener"&gt;AN13767&lt;/A&gt;.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;What advantages does LCU provides?&lt;/STRONG&gt;&amp;nbsp;LCU selects multiple inputs from timers, Pulse Width Modulation (PWM) signals, and Input/Output (I/O) pads, and combines them using a programmable logic function to create output waveforms.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jul 2024 19:58:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Why-LCU-is-used-for-PWM/m-p/1897771#M37110</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2024-07-02T19:58:14Z</dc:date>
    </item>
  </channel>
</rss>