<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックPossible to Erase/Sanitize all memory while running?</title>
    <link>https://community.nxp.com/t5/S32K/Possible-to-Erase-Sanitize-all-memory-while-running/m-p/1895993#M37007</link>
    <description>&lt;P&gt;We are using an S32K148, and our customer has a requirement that the device be able to sanitize all volatile and non-volatile memory upon command, while in operation (no debugger or programmer, should wipe itself).&lt;/P&gt;&lt;P&gt;Is there a way to do this without a bootloader?&amp;nbsp; We presently do not have a bootloader, and using one would add significant complexity.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 28 Jun 2024 14:47:50 GMT</pubDate>
    <dc:creator>m_mishrikey</dc:creator>
    <dc:date>2024-06-28T14:47:50Z</dc:date>
    <item>
      <title>Possible to Erase/Sanitize all memory while running?</title>
      <link>https://community.nxp.com/t5/S32K/Possible-to-Erase-Sanitize-all-memory-while-running/m-p/1895993#M37007</link>
      <description>&lt;P&gt;We are using an S32K148, and our customer has a requirement that the device be able to sanitize all volatile and non-volatile memory upon command, while in operation (no debugger or programmer, should wipe itself).&lt;/P&gt;&lt;P&gt;Is there a way to do this without a bootloader?&amp;nbsp; We presently do not have a bootloader, and using one would add significant complexity.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 28 Jun 2024 14:47:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Possible-to-Erase-Sanitize-all-memory-while-running/m-p/1895993#M37007</guid>
      <dc:creator>m_mishrikey</dc:creator>
      <dc:date>2024-06-28T14:47:50Z</dc:date>
    </item>
    <item>
      <title>Re: Possible to Erase/Sanitize all memory while running?</title>
      <link>https://community.nxp.com/t5/S32K/Possible-to-Erase-Sanitize-all-memory-while-running/m-p/1896625#M37047</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/165923"&gt;@m_mishrikey&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Volatile memories are reinitialized after every reset.&lt;/P&gt;
&lt;P&gt;Non-volatile memories can be erased by sectors from the FTFC controller.&lt;/P&gt;
&lt;P&gt;Except for the EEE backup. The FlexNVM should be pertitioned only once in the life time of the device.&lt;/P&gt;
&lt;P&gt;I'm not sure I understand this use case, can you eleborate on the description?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 01 Jul 2024 10:42:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Possible-to-Erase-Sanitize-all-memory-while-running/m-p/1896625#M37047</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2024-07-01T10:42:32Z</dc:date>
    </item>
    <item>
      <title>Re: Possible to Erase/Sanitize all memory while running?</title>
      <link>https://community.nxp.com/t5/S32K/Possible-to-Erase-Sanitize-all-memory-while-running/m-p/1896642#M37050</link>
      <description>&lt;P&gt;I think it's either trade secret protection,&amp;nbsp; or an extreme cybersecurity requirement.&amp;nbsp; &amp;nbsp;Like in the TV cartoon Inspector Gadget - "This message will self destruct in 5 seconds..."&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 01 Jul 2024 11:12:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Possible-to-Erase-Sanitize-all-memory-while-running/m-p/1896642#M37050</guid>
      <dc:creator>m_mishrikey</dc:creator>
      <dc:date>2024-07-01T11:12:55Z</dc:date>
    </item>
  </channel>
</rss>