<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Setting up freemaster in second core. in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Setting-up-freemaster-in-second-core/m-p/1895863#M37002</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to setup the freemaster in the M7_2 core of s32k358,with the rest of my communication peripherals. but i can't attach the project to that core for some reason. How do I resolve this.&lt;/P&gt;&lt;P&gt;Also, in a different post I had read that both cores have access throughout the whole ram, so there should be no issuesin making such an configuration, right?&lt;/P&gt;</description>
    <pubDate>Fri, 28 Jun 2024 10:25:45 GMT</pubDate>
    <dc:creator>RChatterjee</dc:creator>
    <dc:date>2024-06-28T10:25:45Z</dc:date>
    <item>
      <title>Setting up freemaster in second core.</title>
      <link>https://community.nxp.com/t5/S32K/Setting-up-freemaster-in-second-core/m-p/1895863#M37002</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to setup the freemaster in the M7_2 core of s32k358,with the rest of my communication peripherals. but i can't attach the project to that core for some reason. How do I resolve this.&lt;/P&gt;&lt;P&gt;Also, in a different post I had read that both cores have access throughout the whole ram, so there should be no issuesin making such an configuration, right?&lt;/P&gt;</description>
      <pubDate>Fri, 28 Jun 2024 10:25:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Setting-up-freemaster-in-second-core/m-p/1895863#M37002</guid>
      <dc:creator>RChatterjee</dc:creator>
      <dc:date>2024-06-28T10:25:45Z</dc:date>
    </item>
    <item>
      <title>Re: Setting up freemaster in second core.</title>
      <link>https://community.nxp.com/t5/S32K/Setting-up-freemaster-in-second-core/m-p/1896811#M37059</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/230313"&gt;@RChatterjee&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It is not possible to attach FreeMASTER SDK to the Core 1 since the communication between cores and&amp;nbsp;FreeMASTER should bee made through the Inter-Platform Communication Framework (IPCF). For a better understanding for multicore communication with&amp;nbsp;FreeMASTER refer to&amp;nbsp;S32K324 Triple PMSM Software.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/automotive-development-platforms/s32k-mcu-platforms/s32k324-triple-permanent-magnet-synchronous-motor-control-pmsm-reference-design-board:MCTPTX1AK324" target="_blank" rel="noopener"&gt;S32K324 Triple Permanent Magnet Synchronous Motor Control (PMSM) Reference Design Board&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;B.R.&lt;/P&gt;&lt;P&gt;VaneB&lt;/P&gt;</description>
      <pubDate>Mon, 01 Jul 2024 17:17:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Setting-up-freemaster-in-second-core/m-p/1896811#M37059</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2024-07-01T17:17:26Z</dc:date>
    </item>
  </channel>
</rss>